This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RM57L843 spi与HET初始化冲突问题



背景交代:本人目前在调试的是RM57L843芯片,版本为B版。根据HAL Code Generator配置了SPI接口(SPI1、SPI3、SPI5),调试通过。后有配置了HET模块用于PWM输出,pwm0~PWM7均可输出。后来应用HET_IDE工具配置成13路PWM输出,也可测到所有输出。还配置了ADC1、EMIF、sci1~sci4、CAN1~CAN4、RTI(仅用于定时)。

问题描述:在综合测试时,main函数中完成以下工作:

int main(void)

{

rtiInit();

esmInit();

emif_ASYNC2Init();

gioInit();

sciInit();

adcInit();

canInit();

spiInit();

hetIint();

…………

}

后来测试显示,

情况1:使用HET_IDE生成的HET模块; 如果执行了hetInit();则我的SPI的CLK测不到信号,SPI不正常工作(3组SPI);如果不执行hetInit(),则SPI正常工作。

情况2:使用HET_IDE生成的HET模块; 先执行spiInit();不执行hetInit(); 在执行SPI相关程序,SPI功能正常。SPI功能正常后再执行hetInit()后,在进行SPI相关程序,则SPI功能不正常。

情况3:使用HAL Code Generator配置HET模块。同情况1、2。

后来定位到hetInit()中的  (VOID)memcpy((void *)hetRAM1,(const void*)het1PROGRAM,sizeof(het1PROGRAM));

如果屏蔽掉该语句,则SPI功能正常,但PWM无输出,该语句只是把数组放置到制定RAM中,为何会影响spi的clk.

关于时钟初始化:spi的clk用的是VCLK,het用的是VCLK2,在系统初始化时CCDIS写入的是0X20 除去VCLK2A 未使用,其他均打开了。

请教大神如何解决,或者有没有类似的情况啊

  • 根据您的描述结合数据手册,SPI和N2HET是引脚复用的,个人感觉应该是您的配置有些问题

    请问能否请您给出相关寄存器的配置以及使用的引脚情况?谢谢
  • 您好,感谢您的回复,我刚才又查了一下我的配置。我配置了SPI1 SPI3 SPI5 HET1

    其中SPI1\SPI3\SPI5\HET1的引脚配置为: 

    SPI1 F18 MIBSPI1CLK
    F19 MIBSPI1SIMO[0]
    G18 MIBSPI1SOM1[0]
    R2 MIBSPI1NCS[0]/MIBSPI1SOMI[1]/MII_TXD/ECAP6
    SPI3 V9 MIBSPI3CLK/AD1EXT_SEL/EQEP1A
    V8 MIBSPI3SOMI/AD1EXT_ENA/ECAP2
    V10 MIBSPI3NCS[0]/AD2EVT/EQEP1
    SPI5 H19 MIBSPI5CLK/DMM_DATA[4/MII_TXEN/RMII_TXEN
    J19 MIBSPI5SIMO[0]/DMM_DATA[8]/MII_TXD[1]/RMII_TXD[1]
    J18 MIBSPI5SOMI[0]/DMM_DATA[12]/MII_TXD[0]/RMII_TXD[0]
    E19 MIBSPI5NCS[0]/DMM_DATA[5]/EPWM4A
    HET1 V2 N2HET1[1]/MIBSPI4NENA/N2HET2[8]/EQEP2A
    W5 N2HET1[2]/MIBSPI4SIMO/EPWM3A
    U1 N2HET1[3]/MIBSPI4NCS[0]/N2HET2[10]/EQEP2B
    B12 N2HET1[4]/MIBSPI4NCS[1]/EPWM4B
    V6 N2HET1[5]/MIBSPI4SOMI/N2HET2[12]/EPWM3B
    T1 N2HET1[7]/MIBSPI4NCS[2]/N2HET[14]/EPWM7B
    E18 N2HET1[8]/MIBSPI1SIMO[1]/MII_TXD[3]
    V7 N2HET1[9]/MIBSPI4NCS[3]/N2HET2[16]/EPWM7A
    F19 N2HET1[10]/MIBSPI4NCS[4]/MII_TX_CLK/NTZ1_3
    E3 N2HET1[11]/MIBSPI3NCS[4]/N2HET2[18]/EPWM1SYNCO
    B4 N2HET1[12]/MIBSPI4NCS[5]/MII_CRS/RMII_CRS_DV
    A11 N2HET1[14]
    N1 N2HET1[15]//MIBSPI1NCS[4]/N2HET2[22]/ECAP1

    用配置工具也分别配置了各引脚,未发现有冲突的引脚

  • 您好,补充配置如下:

    SPI配置如下:

    void spiInit(void)
    {
    /* USER CODE BEGIN (2) */
    /* USER CODE END */

    /** @b initialize @b SPI1 */

    /** bring SPI out of reset */
    spiREG1->GCR0 = 0U;
    spiREG1->GCR0 = 1U;

    /** SPI1 master mode and clock configuration */
    spiREG1->GCR1 = (spiREG1->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)1U << 1U) /* CLOKMOD */
    | 1U); /* MASTER */

    /** SPI1 enable pin configuration */
    spiREG1->INT0 = (spiREG1->INT0 & 0xFEFFFFFFU)| (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */

    /** - Delays */
    spiREG1->DELAY = (uint32)((uint32)0U << 24U) /* C2TDELAY */
    | (uint32)((uint32)0U << 16U) /* T2CDELAY */
    | (uint32)((uint32)0U << 8U) /* T2EDELAY */
    | (uint32)((uint32)0U << 0U); /* C2EDELAY */

    /** - Data Format 0 */
    spiREG1->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)74U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 1 */
    spiREG1->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 2 */
    spiREG1->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 3 */
    spiREG1->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - set interrupt levels */
    spiREG1->LVL = (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** - clear any pending interrupts */
    spiREG1->FLG |= 0xFFFFU;

    /** - enable interrupts */
    spiREG1->INT0 = (spiREG1->INT0 & 0xFFFF0000U)
    | (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** @b initialize @b SPI1 @b Port */

    /** - SPI1 Port output values */
    spiREG1->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /** - SPI1 Port direction */
    spiREG1->PC1 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /** - SPI1 Port open drain enable */
    spiREG1->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /** - SPI1 Port pullup / pulldown selection */
    spiREG1->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)1U << 11U) /* SOMI[0] */
    | (uint32)((uint32)1U << 17U) /* SIMO[1] */
    | (uint32)((uint32)1U << 25U); /* SOMI[1] */

    /** - SPI1 Port pullup / pulldown enable*/
    spiREG1->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 25U); /* SOMI[1] */

    /* SPI1 set all pins to functional */
    spiREG1->PC0 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)1U << 11U) /* SOMI[0] */
    | (uint32)((uint32)1U << 17U) /* SIMO[1] */
    | (uint32)((uint32)1U << 25U); /* SOMI[1] */

    /** - Initialize TX and RX data buffer Status */
    g_spiPacket_t[0U].tx_data_status = SPI_READY;
    g_spiPacket_t[0U].rx_data_status = SPI_READY;

    /** - Finally start SPI1 */
    spiREG1->GCR1 = (spiREG1->GCR1 & 0xFEFFFFFFU) | 0x01000000U;

    /** @b initialize @b SPI3 */

    /** bring SPI out of reset */
    spiREG3->GCR0 = 0U;
    spiREG3->GCR0 = 1U;

    /** SPI3 master mode and clock configuration */
    spiREG3->GCR1 = (spiREG3->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)1U << 1U) /* CLOKMOD */
    | 1U); /* MASTER */

    /** SPI3 enable pin configuration */
    spiREG3->INT0 = (spiREG3->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */

    /** - Delays */
    spiREG3->DELAY = (uint32)((uint32)0U << 24U) /* C2TDELAY */
    | (uint32)((uint32)00U << 16U) /* T2CDELAY */
    | (uint32)((uint32)0U << 8U) /* T2EDELAY */
    | (uint32)((uint32)0U << 0U); /* C2EDELAY */

    /** - Data Format 0 */
    spiREG3->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)74U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 1 */
    spiREG3->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)0U << 16U) /* clock phase */
    | (uint32)((uint32)74U << 8U) /* baudrate prescale */
    | (uint32)((uint32)16U << 0U); /* data word length */

    /** - Data Format 2 */
    spiREG3->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)0U << 16U) /* clock phase */
    | (uint32)((uint32)74U << 8U) /* baudrate prescale */
    | (uint32)((uint32)16U << 0U); /* data word length */

    /** - Data Format 3 */
    spiREG3->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)0U << 16U) /* clock phase */
    | (uint32)((uint32)74U << 8U) /* baudrate prescale */
    | (uint32)((uint32)16U << 0U); /* data word length */

    /** - set interrupt levels */
    spiREG3->LVL = (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** - clear any pending interrupts */
    spiREG3->FLG |= 0xFFFFU;

    /** - enable interrupts */
    spiREG3->INT0 = (spiREG3->INT0 & 0xFFFF0000U)
    | (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** @b initialize @b SPI3 @b Port */

    /** - SPI3 Port output values */
    spiREG3->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO */
    | (uint32)((uint32)0U << 11U); /* SOMI */

    /** - SPI3 Port direction */
    spiREG3->PC1 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO */
    | (uint32)((uint32)0U << 11U); /* SOMI */

    /** - SPI3 Port open drain enable */
    spiREG3->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO */
    | (uint32)((uint32)0U << 11U); /* SOMI */

    /** - SPI3 Port pullup / pulldown selection */
    spiREG3->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO */
    | (uint32)((uint32)1U << 11U); /* SOMI */

    /** - SPI3 Port pullup / pulldown enable*/
    spiREG3->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO */
    | (uint32)((uint32)0U << 11U); /* SOMI */

    /* SPI3 set all pins to functional */
    spiREG3->PC0 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO */
    | (uint32)((uint32)1U << 11U); /* SOMI */

    /** - Initialize TX and RX data buffer Status */
    g_spiPacket_t[2U].tx_data_status = SPI_READY;
    g_spiPacket_t[2U].rx_data_status = SPI_READY;

    /** - Finally start SPI3 */
    spiREG3->GCR1 = (spiREG3->GCR1 & 0xFEFFFFFFU) | 0x01000000U;

    /** @b initialize @b SPI5 */

    /** bring SPI out of reset */
    spiREG5->GCR0 = 0U;
    spiREG5->GCR0 = 1U;

    /** SPI5 master mode and clock configuration */
    spiREG5->GCR1 = (spiREG5->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)1U << 1U) /* CLOKMOD */
    | 1U); /* MASTER */

    /** SPI5 enable pin configuration */
    spiREG5->INT0 = (spiREG5->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */

    /** - Delays */
    spiREG5->DELAY = (uint32)((uint32)0U << 24U) /* C2TDELAY */
    | (uint32)((uint32)0U << 16U) /* T2CDELAY */
    | (uint32)((uint32)0U << 8U) /* T2EDELAY */
    | (uint32)((uint32)0U << 0U); /* C2EDELAY */

    /** - Data Format 0 */
    spiREG5->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)0U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 1 */
    spiREG5->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 2 */
    spiREG5->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - Data Format 3 */
    spiREG5->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
    | (uint32)((uint32)0U << 23U) /* parity Polarity */
    | (uint32)((uint32)0U << 22U) /* parity enable */
    | (uint32)((uint32)0U << 21U) /* wait on enable */
    | (uint32)((uint32)0U << 20U) /* shift direction */
    | (uint32)((uint32)0U << 17U) /* clock polarity */
    | (uint32)((uint32)1U << 16U) /* clock phase */
    | (uint32)((uint32)14U << 8U) /* baudrate prescale */
    | (uint32)((uint32)8U << 0U); /* data word length */

    /** - set interrupt levels */
    spiREG5->LVL = (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** - clear any pending interrupts */
    spiREG5->FLG |= 0xFFFFU;

    /** - enable interrupts */
    spiREG5->INT0 = (spiREG5->INT0 & 0xFFFF0000U)
    | (uint32)((uint32)0U << 9U) /* TXINT */
    | (uint32)((uint32)0U << 8U) /* RXINT */
    | (uint32)((uint32)0U << 6U) /* OVRNINT */
    | (uint32)((uint32)0U << 4U) /* BITERR */
    | (uint32)((uint32)0U << 3U) /* DESYNC */
    | (uint32)((uint32)0U << 2U) /* PARERR */
    | (uint32)((uint32)0U << 1U) /* TIMEOUT */
    | (uint32)((uint32)0U << 0U); /* DLENERR */

    /** @b initialize @b SPI5 @b Port */

    /** - SPI5 Port output values */
    spiREG5->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 18U) /* SIMO[2] */
    | (uint32)((uint32)0U << 19U) /* SIMO[3] */
    | (uint32)((uint32)0U << 25U) /* SOMI[1] */
    | (uint32)((uint32)0U << 26U) /* SOMI[2] */
    | (uint32)((uint32)0U << 27U); /* SOMI[3] */

    /** - SPI5 Port direction */
    spiREG5->PC1 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 18U) /* SIMO[2] */
    | (uint32)((uint32)0U << 19U) /* SIMO[3] */
    | (uint32)((uint32)0U << 25U) /* SOMI[1] */
    | (uint32)((uint32)0U << 26U) /* SOMI[2] */
    | (uint32)((uint32)0U << 27U); /* SOMI[3] */


    /** - SPI5 Port open drain enable */
    spiREG5->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 18U) /* SIMO[2] */
    | (uint32)((uint32)0U << 19U) /* SIMO[3] */
    | (uint32)((uint32)0U << 25U) /* SOMI[1] */
    | (uint32)((uint32)0U << 26U) /* SOMI[2] */
    | (uint32)((uint32)0U << 27U); /* SOMI[3] */

    /** - SPI5 Port pullup / pulldown selection */
    spiREG5->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)1U << 11U) /* SOMI[0] */
    | (uint32)((uint32)1U << 17U) /* SIMO[1] */
    | (uint32)((uint32)1U << 18U) /* SIMO[2] */
    | (uint32)((uint32)1U << 19U) /* SIMO[3] */
    | (uint32)((uint32)1U << 25U) /* SOMI[1] */
    | (uint32)((uint32)1U << 26U) /* SOMI[2] */
    | (uint32)((uint32)1U << 27U); /* SOMI[3] */

    /** - SPI5 Port pullup / pulldown enable*/
    spiREG5->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)0U << 1U) /* SCS[1] */
    | (uint32)((uint32)0U << 2U) /* SCS[2] */
    | (uint32)((uint32)0U << 3U) /* SCS[3] */
    | (uint32)((uint32)0U << 4U) /* SCS[4] */
    | (uint32)((uint32)0U << 5U) /* SCS[5] */
    | (uint32)((uint32)0U << 8U) /* ENA */
    | (uint32)((uint32)0U << 9U) /* CLK */
    | (uint32)((uint32)0U << 10U) /* SIMO[0] */
    | (uint32)((uint32)0U << 11U) /* SOMI[0] */
    | (uint32)((uint32)0U << 17U) /* SIMO[1] */
    | (uint32)((uint32)0U << 18U) /* SIMO[2] */
    | (uint32)((uint32)0U << 19U) /* SIMO[3] */
    | (uint32)((uint32)0U << 25U) /* SOMI[1] */
    | (uint32)((uint32)0U << 26U) /* SOMI[2] */
    | (uint32)((uint32)0U << 27U); /* SOMI[3] */

    /* SPI5 set all pins to functional */
    spiREG5->PC0 = (uint32)((uint32)0U << 0U) /* SCS[0] */
    | (uint32)((uint32)1U << 1U) /* SCS[1] */
    | (uint32)((uint32)1U << 2U) /* SCS[2] */
    | (uint32)((uint32)1U << 3U) /* SCS[3] */
    | (uint32)((uint32)1U << 4U) /* SCS[4] */
    | (uint32)((uint32)1U << 5U) /* SCS[5] */
    | (uint32)((uint32)1U << 8U) /* ENA */
    | (uint32)((uint32)1U << 9U) /* CLK */
    | (uint32)((uint32)1U << 10U) /* SIMO[0] */
    | (uint32)((uint32)1U << 11U) /* SOMI[0] */
    | (uint32)((uint32)1U << 17U) /* SIMO[1] */
    | (uint32)((uint32)1U << 18U) /* SIMO[2] */
    | (uint32)((uint32)1U << 19U) /* SIMO[3] */
    | (uint32)((uint32)1U << 25U) /* SOMI[1] */
    | (uint32)((uint32)1U << 26U) /* SOMI[2] */
    | (uint32)((uint32)1U << 27U); /* SOMI[3] */

    /** - Initialize TX and RX data buffer Status */
    g_spiPacket_t[4U].tx_data_status = SPI_READY;
    g_spiPacket_t[4U].rx_data_status = SPI_READY;

    /** - Finally start SPI5 */
    spiREG5->GCR1 = (spiREG5->GCR1 & 0xFEFFFFFFU) | 0x01000000U;

    /* USER CODE BEGIN (3) */
    /* USER CODE END */
    }

    HET配置如下:

    void hetInit(void)
    {
    /** @b initialize @b HET */

    /** - Set HET pins default output value */
    hetREG1->DOUT = (uint32)((uint32)0U << 31U)
    | (uint32)((uint32)0U << 30U)
    | (uint32)((uint32)0U << 29U)
    | (uint32)((uint32)0U << 28U)
    | (uint32)((uint32)0U << 27U)
    | (uint32)((uint32)0U << 26U)
    | (uint32)((uint32)0U << 25U)
    | (uint32)((uint32)0U << 24U)
    | (uint32)((uint32)0U << 23U)
    | (uint32)((uint32)0U << 22U)
    | (uint32)((uint32)0U << 21U)
    | (uint32)((uint32)0U << 20U)
    | (uint32)((uint32)0U << 19U)
    | (uint32)((uint32)0U << 18U)
    | (uint32)((uint32)0U << 17U)
    | (uint32)((uint32)0U << 16U)
    | (uint32)((uint32)0U << 15U)
    | (uint32)((uint32)0U << 14U)
    | (uint32)((uint32)0U << 13U)
    | (uint32)((uint32)0U << 12U)
    | (uint32)((uint32)0U << 11U)
    | (uint32)((uint32)0U << 10U)
    | (uint32)((uint32)0U << 9U)
    | (uint32)((uint32)0U << 8U)
    | (uint32)((uint32)0U << 7U)
    | (uint32)((uint32)0U << 6U)
    | (uint32)((uint32)0U << 5U)
    | (uint32)((uint32)0U << 4U)
    | (uint32)((uint32)0U << 3U)
    | (uint32)((uint32)0U << 2U)
    | (uint32)((uint32)0U << 1U)
    | (uint32)((uint32)0U << 0U);

    /** - Set HET pins direction */
    hetREG1->DIR = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00008000U
    | (uint32) 0x00004000U
    | (uint32) 0x00000000U
    | (uint32) 0x00001000U
    | (uint32) 0x00000800U
    | (uint32) 0x00000400U
    | (uint32) 0x00000200U
    | (uint32) 0x00000100U
    | (uint32) 0x00000080U
    | (uint32) 0x00000040U
    | (uint32) 0x00000020U
    | (uint32) 0x00000010U
    | (uint32) 0x00000008U
    | (uint32) 0x00000004U
    | (uint32) 0x00000002U
    | (uint32) 0x00000000U;

    /** - Set HET pins open drain enable */
    hetREG1->PDR = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U;

    /** - Set HET pins pullup/down enable */
    hetREG1->PULDIS = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U;

    /** - Set HET pins pullup/down select */
    hetREG1->PSL = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U;

    /** - Set HET pins high resolution share */
    hetREG1->HRSH = (uint32) 0x00008000U
    | (uint32) 0x00004000U
    | (uint32) 0x00002000U
    | (uint32) 0x00001000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000002U
    | (uint32) 0x00000000U;

    /** - Set HET pins AND share */
    hetREG1->AND = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U;

    /** - Set HET pins XOR share */
    hetREG1->XOR = (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U
    | (uint32) 0x00000000U;

    /* USER CODE BEGIN (1) */

    /* USER CODE END */

    /** - Setup prescaler values
    * - Loop resolution prescaler
    * - High resolution prescaler
    */
    hetREG1->PFR = (uint32)((uint32) 6U << 8U)
    | ((uint32) 0U);


    /** - Parity control register
    * - Enable/Disable Parity check
    */
    hetREG1->PCR = (uint32) 0x00000005U;

    /** - Fill HET RAM with opcodes and Data */
    /** - "x" in "HET_INITx_PST" denote the HET module Instance
    * Valid range of x - 0 to 9
    * For HET1 module x = 0
    * Refer HET assembler User guide for more Info
    */
    /*SAFETYMCUSW 94 S MR:11.1,11.2,11.4 <APPROVED> "HET RAM Fill from the table - Allowed as per MISRA rule 11.2" */
    /*SAFETYMCUSW 95 S MR:11.1,11.4 <APPROVED> "HET RAM Fill from the table - Allowed as per MISRA rule 11.2" */
    /*SAFETYMCUSW 95 S MR:11.1,11.4 <APPROVED> "HET RAM Fill from the table - Allowed as per MISRA rule 11.2" */
    (void)memcpy((void*)hetRAM1, (void*)HET_INIT0_PST, sizeof(HET_INIT0_PST));

    /** - Setup interrupt priority level */
    hetREG1->PRY = 0xFFFFFFFF;

    /** - Enable interrupts */
    hetREG1->INTENAC = 0xFFFFFFFFU;
    hetREG1->INTENAS = (uint32) 0x80000000U
    | (uint32) 0x40000000U
    | (uint32) 0x20000000U
    | (uint32) 0x10000000U
    | (uint32) 0x08000000U
    | (uint32) 0x04000000U
    | (uint32) 0x02000000U
    | (uint32) 0x01000000U
    | (uint32) 0x00800000U
    | (uint32) 0x00400000U
    | (uint32) 0x00200000U
    | (uint32) 0x00100000U
    | (uint32) 0x00080000U
    | (uint32) 0x00040000U
    | (uint32) 0x00020000U
    | (uint32) 0x00010000U
    | (uint32) 0x00008000U
    | (uint32) 0x00004000U
    | (uint32) 0x00002000U
    | (uint32) 0x00001000U
    | (uint32) 0x00000800U
    | (uint32) 0x00000400U
    | (uint32) 0x00000200U
    | (uint32) 0x00000100U
    | (uint32) 0x00000080U
    | (uint32) 0x00000040U
    | (uint32) 0x00000020U
    | (uint32) 0x00000010U
    | (uint32) 0x00000008U
    | (uint32) 0x00000004U
    | (uint32) 0x00000000U
    | (uint32) 0x00000001U;


    /** - Setup control register
    * - Enable output buffers
    * - Ignore software breakpoints
    * - Master or Slave Clock Mode
    * - Enable HET
    */
    hetREG1->GCR = ( 0x00000001U
    | (uint32)((uint32)0U << 24U)
    | (uint32)((uint32)1U << 16U)
    | (0x00020000U));


    /* USER CODE BEGIN (4) */
    /* USER CODE END */

    }

    其中红色标注部分若屏蔽掉,则SPI功能正常,若不屏蔽则SPI与HET有冲突

  • 您好,我的问题已解决。

    解决方法: 之前在配置SPI时,有部分引脚与HET复用(选择的功能为N2HET)  如:

    E18 N2HET1[8]/MIBSPI1SIMO[1]/MII_TXD[3]

    B4 N2HET1[12]/MIBSPI4NCS[5]/MII_CRS/RMII_CRS_DV

    N1 N2HET1[15]//MIBSPI1NCS[4]/N2HET2[22]/ECAP1

    ,SPI配置中该引脚不使用,未使能也未输出。引脚类型选择的时SPI模式。

    现在将这些引脚改为GIO模式后,我之前描述的现象就不存在了。

    我之前先进行spiInit();测试SPI功能正常,在进行hetInit(),测试HET功能正常。之后再进行SPI测试后,功能就异常了。如果再进行spiInit();功能依然不正常。  如果是该引脚类型(与HET复用的引脚,就算配置为HET功能,在SPI中也要配置为GIO模式)引起了该冲突的话,那按道理来说,我再次进行spiInit()后,我的SPI功能就应该恢复正常啊,为何会出现我之前描述的此类现象。是否为芯片级的BUG?

  • 很高兴您能解决问题!

    关于您提到的引脚复用问题,建议您看一下 www.ti.com.cn/.../spnu562a.pdf



    I/O Multiplexing and Control Module (IOMM)
  • 以及 6.7.13 PINMMRnn: Input Pin Multiplexing Control Registers 和 6.7.12 PINMMRnn: Output Pin Multiplexing Control Registers