大家好,我是一名初学者,就是现在我在学习tms570ls0914和tps65381配置的问题,但是有一些基础问题不是很清楚,想求助一下大家
1、对于ccs里面的很多函数中出现的mibspi-t*怎么理解,翻译过来是mibspi模块基址,但我不是很清楚这个模块基址是什么意思(比如函数mibspiset(mibspi,group,data)里面group和data都好理解,就是这个mibspi该怎么理解)
2、之前看了几个官方的例程,但是例程是rm46和tps65381之间的配置,想问一下大家有没有关于tps65381给tms570ls通过spi喂狗的例程
3、在RM46与tps65381相连的程序里,有用ecmpinit函数强制tps65381保持在诊断状态,如果mcu是tms570ls,这个ecmpinit函数是否依然有效
4、对从芯片的寄存器进行操作时,很多寄存器都支持读写两个操作,对寄存器进行读写操作时 ,分别要用什么代码实现,我之前以为是利用spisetdata()函数写一个16bit的数发送过去就好,但是看了很多例程好像并没有用这种方式,我想问一下,如果对从芯片寄存器配置的话一般要怎么实现