This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299EEG FE Rev A與MSP432P401R的SPI傳輸



我是SPI 的初學者,看到官方CCS的範例都是SPI的3線傳輸的範例。

請問ADS1299EEG FE Rev A與MSP432P401R的SPI傳輸是不是只能使用4線傳輸?

他們之間的SPI傳輸又該如何撰寫?

有什麼方式可以讓我更快入手的嗎?

  • 您可以看一下ADS1229的数据手册内的说明 www.ti.com/.../ads1299.pdf

    The SPI-compatible serial interface consists of four signals: CS, SCLK, DIN, and DOUT.

    使用的是4线的SPI

    关于MSP432的SPI例程,您可以下载 www.ti.com/.../SIMPLELINK-MSP432-SDK

    后在其安装文件夹内找到

    <SDK_INSTALL_DIR>\examples\rtos\MSP_EXP432P401R\drivers\spimaster

    4线SPI的话可以使用 SPI_selectFourPinFunctionality 来使能
  • SPI_selectFourPinFunctionality  這個如何使用?

    可以舉例說明一下嗎?

  • 您可以参考一下下面的链接,有详细的函数说明

    dev.ti.com/.../group__spi__api.html
  • 我現在使用兩塊MSP432P401R,我想設定成4線傳輸,並且要讓MASTER接收SLAVE傳送來的資料,可是我不知道我的錯誤在哪,CLOCK沒有任何訊號,我的代碼如下:


    MASTER:
    /* DriverLib Includes */
    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>

    /* Standard Includes */
    #include <stdint.h>
    #include <stdbool.h>

    /* Statics */
    //static volatile uint8_t RXData = 0;
    //static uint8_t TXData = 0;
    static volatile uint8_t transmitData = 0x01, receiveData = 0x00;
    //![Simple SPI Config]
    /* SPI Master Configuration Parameter */
    const eUSCI_SPI_MasterConfig spiMasterConfig =
    {
    EUSCI_B_SPI_CLOCKSOURCE_SMCLK, // SMCLK Clock Source
    3000000, // SMCLK = DCO = 3MHZ
    500000, // *** = 500khz
    EUSCI_B_SPI_MSB_FIRST, // MSB First
    EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase
    EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // High polarity
    //EUSCI_B_SPI_3PIN // 3Wire SPI Mode
    EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH // 4Wire SPI Mode
    };
    //![Simple SPI Config]

    int main(void)
    {
    /* Halting WDT */
    WDT_A_holdTimer();

    //![Simple SPI Example]
    /* Selecting P1.5 P1.6 and P1.7 in SPI mode */
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
    GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
    // GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5,
    // GPIO_PIN2,GPIO_PRIMARY_MODULE_FUNCTION);

    //CS
    GPIO_setAsOutputPin(GPIO_PORT_P4,GPIO_PIN3);
    GPIO_setOutputHighOnPin(GPIO_PORT_P4,GPIO_PIN3);
    //CS

    /* Configuring SPI in 3wire master mode */
    SPI_initMaster(EUSCI_B0_BASE, &spiMasterConfig);

    /* Enable SPI module */
    SPI_enableModule(EUSCI_B0_BASE);

    /* Enabling interrupts */
    SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
    Interrupt_enableSleepOnIsrExit();
    Interrupt_enableInterrupt(INT_EUSCIB0);

    //![Simple SPI Example]
    //TXData = 0x01;
    GPIO_setOutputLowOnPin(GPIO_PORT_P4,GPIO_PIN3);
    /* Polling to see if the TX buffer is ready */
    while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_RECEIVE_INTERRUPT)));

    /* Transmitting data to slave */
    //SPI_transmitData(EUSCI_B0_BASE, TXData);
    GPIO_setOutputHighOnPin(GPIO_PORT_P4,GPIO_PIN3);
    //Interrupt_enableMaster();
    PCM_gotoLPM0();
    __no_operation();
    }

    //******************************************************************************
    //
    //This is the EUSCI_B0 interrupt vector service routine.
    //
    //******************************************************************************
    void EUSCIB0_IRQHandler(void)
    {
    //uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
    //uint32_t jj;

    uint32_t status;

    status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);


    SPI_clearInterruptFlag(EUSCI_B0_BASE, status);

    if(status & EUSCI_B_SPI_RECEIVE_INTERRUPT)
    {
    /* USCI_B0 TX buffer ready? */
    while (!(SPI_getInterruptStatus(EUSCI_B0_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT)));
    //GPIO_setOutputLowOnPin(GPIO_PORT_P5,GPIO_PIN2);
    //RXData = SPI_receiveData(EUSCI_B0_BASE);

    /* Send the next data packet */
    //SPI_transmitData(EUSCI_B0_BASE, ++TXData);
    // SPI_transmitData(EUSCI_B0_BASE, transmitData++);

    /* Delay between transmissions for slave to process information */
    //for(jj=50;jj<50;jj++);
    receiveData = SPI_receiveData(EUSCI_B0_BASE);
    //GPIO_setOutputHighOnPin(GPIO_PORT_P5,GPIO_PIN2);
    }

    }



    SLAVE:
    /* DriverLib Includes */
    #include <ti/devices/msp432p4xx/driverlib/driverlib.h>

    /* Statics */
    //static volatile uint8_t transmitData = 0x01, receiveData = 0x00;
    static volatile uint8_t RXData = 0;
    static uint8_t TXData = 0;
    /* SPI Slave Configuration Parameter */
    const eUSCI_SPI_SlaveConfig spiSlaveConfig =
    {
    EUSCI_B_SPI_MSB_FIRST, // MSB First
    EUSCI_B_SPI_PHASE_DATA_CHANGED_ONFIRST_CAPTURED_ON_NEXT, // Phase
    EUSCI_B_SPI_CLOCKPOLARITY_INACTIVITY_HIGH, // Normal Polarity
    //EUSCI_B_SPI_3PIN // 3wire mode
    EUSCI_B_SPI_4PIN_UCxSTE_ACTIVE_HIGH, // 4線SPI模式

    };

    int main(void)
    {
    /* Stop watchdog timer */
    WDT_A_holdTimer();

    /* Selecting P1.1 P1.2 and P1.3 in SPI mode */
    GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P1,
    GPIO_PIN5 | GPIO_PIN6 | GPIO_PIN7, GPIO_PRIMARY_MODULE_FUNCTION);
    // GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P5,
    // GPIO_PIN2,SPI_selectFourPinFunctionality );
    //CS
    GPIO_setAsOutputPin(GPIO_PORT_P4,GPIO_PIN3);
    GPIO_setOutputHighOnPin(GPIO_PORT_P4,GPIO_PIN3);
    //CS
    /* Initialize slave to MSB first, inactive high clock polarity and
    * 3 wire SPI */
    SPI_initSlave(EUSCI_B0_BASE, &spiSlaveConfig);

    /* Enable the SPI module */
    SPI_enableModule(EUSCI_B0_BASE);

    /* Enable Receive interrupt */
    SPI_enableInterrupt(EUSCI_B0_BASE, EUSCI_B_SPI_RECEIVE_INTERRUPT);
    Interrupt_enableSleepOnIsrExit();
    Interrupt_enableInterrupt(INT_EUSCIB0);

    //![Simple SPI Example]
    GPIO_setOutputLowOnPin(GPIO_PORT_P4,GPIO_PIN3);
    TXData = 0x01;

    /* Polling to see if the TX buffer is ready */
    while (!(SPI_getInterruptStatus(EUSCI_B0_BASE,EUSCI_B_SPI_TRANSMIT_INTERRUPT)));

    /* Transmitting data to slave */
    SPI_transmitData(EUSCI_B0_BASE, TXData);

    Interrupt_enableMaster();
    GPIO_setOutputHighOnPin(GPIO_PORT_P4,GPIO_PIN3);
    PCM_gotoLPM0();
    __no_operation();

    }

    //******************************************************************************
    //
    //This is the EUSCI_B0 interrupt vector service routine.
    //
    //******************************************************************************
    void EUSCIB0_IRQHandler(void)
    {
    //uint32_t status;
    uint32_t status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
    uint32_t jj;

    //status = SPI_getEnabledInterruptStatus(EUSCI_B0_BASE);
    //SPI_clearInterruptFlag(EUSCI_B0_BASE, status);

    if(status & EUSCI_B_SPI_RECEIVE_INTERRUPT)
    {
    /* USCI_B0 TX buffer ready? */
    while (!(SPI_getInterruptStatus(EUSCI_B0_BASE, EUSCI_B_SPI_TRANSMIT_INTERRUPT)));

    // RXData = SPI_receiveData(EUSCI_B0_BASE);
    /* Transmit data to master */
    //SPI_transmitData(EUSCI_B0_BASE, transmitData++);
    SPI_transmitData(EUSCI_B0_BASE, ++TXData);

    //Receive data from master
    //receiveData = SPI_receiveData(EUSCI_B0_BASE);
    for(jj=50;jj<50;jj++);

    }
    }
  • 代码太长,就不一一看了,CLOCK沒有任何訊號,说明你的SPI外设没有初始化完成,你是否用官方的代码例程进行了测试呢?这样可以找到你代码的错误在哪里。
  • 範例程式碼主要是MSTER發送資料給SLAVE
    我的代碼是將SLAVE發送資料給MASTER接收
    我只有將兩個官方範例代碼乎鄉修改而已
    我最後的目的是要MASTER接收SLAVE傳送的資料