Other Parts Discussed in Thread: HALCOGEN
你好,我想咨询一下,我用safety diagnostic library初始化了flash的ecc功能,库中有函数或者有其他办法可以软件触发ecc错误使esm模块响应吗?SL_SAELFTEST_FLASH函数可以通过参数设置实现触发ecc的错误码?
我使用的是RM48的开发板,HALCOGEN生成的驱动库,添加了safety diagnostic library
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: HALCOGEN
你好,我想咨询一下,我用safety diagnostic library初始化了flash的ecc功能,库中有函数或者有其他办法可以软件触发ecc错误使esm模块响应吗?SL_SAELFTEST_FLASH函数可以通过参数设置实现触发ecc的错误码?
我使用的是RM48的开发板,HALCOGEN生成的驱动库,添加了safety diagnostic library
您可以查看sl_esm.c
/*******************************************************************************
**+--------------------------------------------------------------------------+**
**| |**
**| Copyright (c) 2012 Texas Instruments Incorporated |**
**| ALL RIGHTS RESERVED |**
**| |**
**| Permission is hereby granted to licensees of Texas Instruments |**
**| Incorporated (TI) products to use this computer program for the sole |**
**| purpose of implementing a licensee product based on TI products. |**
**| No other rights to reproduce, use, or disseminate this computer |**
**| program, whether in part or in whole, are granted. |**
**| |**
**| TI makes no representation or warranties with respect to the |**
**| performance of this computer program, and specifically disclaims |**
**| any responsibility for any damages, special or consequential, |**
**| connected with the use of this program. |**
**| |**
**+--------------------------------------------------------------------------+**
*******************************************************************************/
/**
* @file sl_esm.c
* @version 2.4.0
* @brief File contains esm handling and interrupt handlers for esm errors
*
* @details This file implements interrupt handlers for the esmHigh and esmLow interrupts\n
* the esm group 2 and group 1 handlers have been implemented which can be further extended\n
* depending on the end application.It provides the Init function which updates the application\n
* callback function and the interrupt handlers for esmHigh and esmLow interrupt.It also provides\n
* API's which provide the information on the nError pin status
*/
/* Comments regarding various justifications for deviation from MISRA-C coding guidelines
* are provided at the bottom of the file
*/
#include <sl_api.h>
#include <sl_priv.h>
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
#include <sl_reg_flash.h>
#endif
#if (FUNCTION_PROFILING_ENABLED != 0)
#include <sl_sys_pmu.h>
#endif
#ifdef __IAR_SYSTEMS_ICC__
__fiq
#endif
static
void sl_esm_high_intr_handler(void);
#ifdef __IAR_SYSTEMS_ICC__
__irq
#endif
static
void sl_esm_low_intr_handler(void);
static
void esmGroup1Handler(uint8 esmChannel);
static
void esmGroup2Handler(uint8 esmChannel);
/*SAFETYMCUSW 298 S MR:- <APPROVED> Comment_1*/
#ifdef __IAR_SYSTEMS_ICC__
#pragma location=".noinit"
static ESM_Application_Callback ESM_AppCallback;
#endif
#ifdef __TI_COMPILER_VERSION__
static ESM_Application_Callback ESM_AppCallback;
#endif
static uint32 callbackCancelCount = 0u;
/*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/
void SL_ESM_Init(ESM_Application_Callback appCallback)
{
#ifdef __TI_COMPILER_VERSION__
/*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/
sl_vimRAM->ISR[1U] = &sl_esm_high_intr_handler;
sl_vimRAM->ISR[21U] = &sl_esm_low_intr_handler;
#endif
#ifdef __IAR_SYSTEMS_ICC__
/*SAFETYMCUSW 61 D MR: 8.10,8.11 <APPROVED> Comment_2*/
sl_vimRAM->ISR[1] = (sl_t_isrFuncPTR)&sl_esm_high_intr_handler;
sl_vimRAM->ISR[21] = (sl_t_isrFuncPTR)&sl_esm_low_intr_handler;
#endif
ESM_AppCallback = appCallback;
}
boolean SL_ESM_nERROR_Active(void)
{
boolean retval = FALSE;
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
if(ESM_ERROR_PIN_OFF == BF_GET(sl_esmREG->EPSR, BF_EPSF_START, BF_EPSF_LENGTH)) {
retval = FALSE;
}
else {
retval = TRUE;
}
return(retval);
}
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/
#ifdef __TI_COMPILER_VERSION__
#pragma CODE_STATE(sl_esm_high_intr_handler, 32)
#endif
#ifdef __IAR_SYSTEMS_ICC__
__arm
#endif
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/
#ifdef __TI_COMPILER_VERSION__
#pragma INTERRUPT(sl_esm_high_intr_handler, FIQ)
#endif
#ifdef __IAR_SYSTEMS_ICC__
__fiq
#endif
static void sl_esm_high_intr_handler(void)
{
register uint8 esmOffH,esmChannel;
#if (FUNCTION_PROFILING_ENABLED != 0)
register uint32 entrytick=0u;
entrytick = _sl_pmuGetCycleCount_();
#endif
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
esmOffH = (uint8) sl_esmREG->IOFFHR;
if (0u != esmOffH) {
esmOffH--;
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
if (esmOffH >= 128u && esmOffH < 160u) {
/* Group 1 channel 64 to 95 */
esmChannel = esmOffH - 64u;
esmGroup1Handler(esmChannel);
} else
#endif
if (esmOffH >= 96u) {
/* Shouldn't be here... */
/* Misra C fix 477S added to make the else part non empty */
esmOffH = esmOffH;
}
else if (esmOffH >= 64u) {
/* Group 1 channel 32 to 63 */
esmChannel = esmOffH - 32u;
esmGroup1Handler(esmChannel);
}
else if (esmOffH >= 32u) {
/* Group 2 channel 0 to 31 */
esmChannel = esmOffH - 32u;
esmGroup2Handler(esmChannel);
}
else if (esmOffH > 0u) {
/* Group 1 channel 0 to 31 */
esmChannel = esmOffH;
esmGroup1Handler(esmChannel);
}
else {
/* Shouldn't be here... */
/* Misra C fix 477S added to make the else part non empty */
esmOffH++;
}
}
else {
/* Shouldn't get here... */
/* Misra C fix 477S added to make the else part non empty */
esmOffH++;
}
#if (FUNCTION_PROFILING_ENABLED != 0)
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
if ((esmChannel != ESM_G2ERR_B0TCM_ADDPAR) &&
(esmChannel != ESM_G2ERR_B1TCM_ADDPAR)) {
#endif
if(SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick == 0U )
{
SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick = entrytick;
SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_exittick = _sl_pmuGetCycleCount_();
}
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
}
#endif
#endif
}
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/
#ifdef __TI_COMPILER_VERSION__
#pragma CODE_STATE(sl_esm_low_intr_handler, 32)
#endif
#ifdef __IAR_SYSTEMS_ICC__
__arm
#endif
/*SAFETYMCUSW 69 S MR:3.4 <APPROVED> Comment_3*/
#ifdef __TI_COMPILER_VERSION__
#pragma INTERRUPT(sl_esm_low_intr_handler, IRQ)
#endif
#ifdef __IAR_SYSTEMS_ICC__
__irq
#endif
static void sl_esm_low_intr_handler(void) {
register uint8 esmOffL,esmChannel;
#if (FUNCTION_PROFILING_ENABLED != 0)
register uint32 entrytick=0u;
entrytick = _sl_pmuGetCycleCount_();
#endif
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
esmOffL = ((uint8)sl_esmREG->IOFFLR - (uint8)1u);
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
if ((esmOffL >= 128U) && (esmOffL < 160U))
{
/* Group 1 channel 64 to 95 */
esmChannel = esmOffL-64u;
esmGroup1Handler(esmChannel);
}
else {
#endif
if ((esmOffL >= 64U) && (esmOffL < 96U))
{
/* Group 1 channel 32 to 63 */
esmChannel = esmOffL-32u;
esmGroup1Handler(esmChannel);
}
else if( esmOffL < 32U){
/* Group 1 channel 0 to 31 */
esmChannel = esmOffL;
esmGroup1Handler(esmChannel);
}
else {
/* Shouldn't be here... */
/* Misra C fix 477S added to make the else part non empty */
esmOffL++;
}
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
}
#endif
#if (FUNCTION_PROFILING_ENABLED != 0)
if(SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick == 0U )
{
SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_entrytick = entrytick;
SL_Profile_Struct[SL_Active_Profile_Testtype-TESTTYPE_MIN].esm_exittick = _sl_pmuGetCycleCount_();
}
#endif
return;
}
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
#include "sl_reg_flash.h"
#endif
#ifdef __TI_COMPILER_VERSION__
#pragma WEAK(esmGroup2Handler)
#endif
static void esmGroup2Handler (uint8 esmChannel)
{
boolean cancelCallback = FALSE;
register uint32 callbkParam1 = 0u, callbkParam2 = 0u, callbkParam3 = 0u;
/* No need to clear ESM bit since reading ESMOFFH automatically clears the status bit */
switch (esmChannel) {
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
/** L2RAM Uncorrectable Error */
case ESM_G2ERR_L2RAMW_UNCORR_B:
if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT) ||
TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_2BIT) ) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** CCMR5 CPU COMPARE Error */
case ESM_G2ERR_CCMR5_CPUCOMP_ERR:
/* No additional parameters available */
callbkParam1 = 0u;
/* Error is intentional due to diagnostic test - Clear the module
* error */
ccmr5fREG1->_CCMSR1 = CCMR5F_CCMSR_CMPE;
/* Cancel callback if this was intentional */
if (TRUE == SL_FLAG_GET(CCMR5F_CPUCOMP_ERROR_FORCING_TEST)) {
if (TRUE == SL_FLAG_GET(VIM_SOFTWARE_TEST)){
vimTestFlag = TRUE;
}
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** CCMR5 VIM COMPARE Error */
case ESM_G2ERR_CCMR5_VIMCOMP_ERR:
/* No additional parameters available */
callbkParam1 = 0u;
/* Error is intentional due to diagnostic test - Clear the module
* error */
ccmr5fREG1->_CCMSR2 = CCMR5F_CCMSR_CMPE;
/* Cancel callback if this was intentional */
if (TRUE == SL_FLAG_GET(CCMR5F_VIMCOMP_ERROR_FORCING_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** CCMR5 Power Domain monitor Error */
case ESM_G2ERR_CCMR5_PDCOMP_ERR:
/* No additional parameters available */
callbkParam1 = 0u;
/* Error is intentional due to diagnostic test - Clear the module
* error */
ccmr5fREG1->_CCMSR3 = CCMR5F_CCMSR_CMPE;
/* Cancel callback if this was intentional */
if (TRUE == SL_FLAG_GET(CCMR5F_PDCOMP_ERROR_FORCING_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** CPU1 AXIM Bus Monitor failure */
case ESM_G2ERR_CCMR5_INMCOMP_ERR:
/* No additional parameters available */
callbkParam1 = 0u;
/* Error is intentional due to diagnostic test - Clear the module
* error */
ccmr5fREG1->_CCMSR4 = CCMR5F_CCMSR_CMPE;
/* Cancel callback if this was intentional */
if (TRUE == SL_FLAG_GET(CCMR5F_INMCOMP_ERROR_FORCING_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
#endif
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
/** CCMR4 Compare Error */
case ESM_G2ERR_CCMR4_COMP:
/* No additional parameters available */
callbkParam1 = 0u;
/* Clear the module error */
ccmr4fREG1->_CCMSR = CCMR4F_CCMSR_CMPE;
/* Cancel callback if this was intentional */
if (TRUE == SL_FLAG_GET(CCMR4F_ERROR_FORCING_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** F021Flash Uncorrectable Error */
case ESM_G2ERR_FMC_UNCORR:
if (TRUE == SL_FLAG_GET(FLASH_ADDRESS_PARITY_SELF_TEST)) {
/* Disable Parity Overrun and enable only Bus Parity Enable */
sl_flashWREG->FPAROVR = F021F_FPAROVR_BUS_PAR_ENABLE;
/* Clear Diagnostics enable key and Disable Diagnostics Mode */
sl_flashWREG->FDIAGCTRL &= (~(F021F_FDIAGCTRL_DIAG_EN_KEY | F021F_FDCTRL_DMODE_TEST_MODE));
callbackCancelCount++;
cancelCallback = TRUE;
}
if (TRUE == SL_FLAG_GET(FLASH_ADDRESS_PARITY_FAULT_INJECT)) {
/* Disable Parity Overrun and enable only Bus Parity Enable */
sl_flashWREG->FPAROVR = F021F_FPAROVR_BUS_PAR_ENABLE;
/* Clear Diagnostics enable key and Disable Diagnostics Mode */
sl_flashWREG->FDIAGCTRL &= (~(F021F_FDIAGCTRL_DIAG_EN_KEY | F021F_FDCTRL_DMODE_TEST_MODE));
}
/* Flash Un-correctable error, capture the error address */
callbkParam1 = sl_flashWREG->FUNCERRADD;
/* No status to clear here */
break;
/** RAM even bank (B0TCM) - uncorrectable Error */
case ESM_G2ERR_B0TCM_UNCORR:
if (TRUE == SL_FLAG_GET(SRAM_RADECODE_DIAGNOSTICS)) {
if (TRUE == SL_FLAG_GET(VIM_SOFTWARE_TEST)){
vimTestFlag = TRUE;
}
callbackCancelCount++;
cancelCallback = TRUE;
}
callbkParam1 = sl_tcram1REG->RAMUERRADDR;
/* No status to clear here */
break;
/** RAM odd bank (B1TCM) - uncorrectable Error */
case ESM_G2ERR_B1TCM_UNCORR:
if (TRUE == SL_FLAG_GET(SRAM_RADECODE_DIAGNOSTICS)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
callbkParam1 = sl_tcram2REG->RAMUERRADDR;
/* No status to clear here */
break;
/** RAM even bank (B0TCM) - Address bus Parity Error */
case ESM_G2ERR_B0TCM_ADDPAR:
if (TRUE == SL_FLAG_GET(SRAM_PAR_ADDR_CTRL_SELF_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
callbkParam1 = sl_tcram1REG->RAMPERADDR;
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam2 = (sl_tcram1REG->RAMERRSTATUS
& (TCRAM_RAMERRSTAT_WADDRPAR_FAIL | TCRAM_RAMERRSTAT_RADDRPAR_FAIL));
callbkParam3 = (uint32) 0u;
/* Clear the WADDR/RADDR PAR Fail bits in TCM Regs */
break;
/** RAM odd bank (B0TCM) - Address bus Parity Error */
case ESM_G2ERR_B1TCM_ADDPAR:
if (TRUE == SL_FLAG_GET(SRAM_PAR_ADDR_CTRL_SELF_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
callbkParam1 = sl_tcram2REG->RAMPERADDR;
/* No status to clear here */
break;
/** TCM - ECC live lock detect */
case ESM_G2ERR_FLASH_LIVLCK:
callbkParam1 = 0u;
/* No status to clear here */
break;
/** Windowed Watchdog (WWD) violation */
case ESM_G2ERR_RTI_WWD_NMI:
callbkParam1 = 0u;
/* No status to clear here */
break;
#endif
default:
/* nothing here - comment to avoid misra-c warning */
break;
}
/* Call application callback only if it's registered & if it's not masked */
/* the MSB of contains information regarding group and LSB contains the esm channel number*/
if ((0u != ESM_AppCallback) && ((boolean)(FALSE) == cancelCallback)) {
(*(ESM_AppCallback))((uint32)(ESM_GRP2_MASK | esmChannel), callbkParam1, callbkParam2, callbkParam3);
}
return;
}
#ifdef __TI_COMPILER_VERSION__
#pragma WEAK(esmGroup1Handler)
#endif
static
void esmGroup1Handler(uint8 esmChannel)
{
boolean cancelCallback = FALSE;
register uint32 callbkParam1 = 0u, callbkParam2 = 0u, callbkParam3 = 0u;
switch (esmChannel) {
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
/** F021 Flash Correctabe error (bus1 & bus2) & non-EEPROM **/
case ESM_G1ERR_FMC_CORR:
if (TRUE == SL_FLAG_GET(FLASH_ECC_TEST_MODE_1BIT)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/* Retrieve the callback parameters */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (sl_flashWREG->FCORERRCNT & 0x0000FFFFu);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam2 = (sl_flashWREG->FCORERRADD);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam3 = (sl_flashWREG->FCORERRPOS & 0x000003FFu);
break;
/** PLL1 Slip error **/
case ESM_G1ERR_PLL1_SLIP:
/** Store the callback parameters & reset the status registers */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (uint32)((uint32)(sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u);
break;
/** LPOCLK Detect error */
case ESM_G1ERR_CLOCKMON_INTR:
break;
/** VIM Parity Error **/
case ESM_G1ERR_VIMRAM_PARITY:
if (TRUE == SL_FLAG_GET(VIM_SRAM_PARITY_TEST)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/* Extract the parameters & clear the flag */
callbkParam1 = SL_VIM_ADDERR;
SL_VIM_PARFLG = 1u;
break;
/** B0TCM ECC Correctable error **/
case ESM_G1ERR_B0TCM_CORRERR:
if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/* Call application if this error was _not_ intentional (self-test) */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (sl_tcram1REG->RAMSERRADDR);
break;
/** B1TCM ECC Correctable error **/
case ESM_G1ERR_B1TCM_CORRERR:
if (TRUE == SL_FLAG_GET(SRAM_ECC_ERROR_FORCING_1BIT)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (sl_tcram2REG->RAMSERRADDR);
/* Call application if this error was _not_ intentional (self-test) */
break;
/** DCC Error */
case ESM_G1ERR_DCC1_ERR:
callbkParam1 = sl_dccREG1->CNT0;
callbkParam2 = sl_dccREG1->CNT1;
/* Clear Error Flag */
sl_dccREG1->STAT = DCC_DCCSTAT_ERR_FLG;
break;
/** CCMR4 Self-Test Compare error */
case ESM_G1ERR_CCMR4_SELFTEST:
/*ccmr4f selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
if (TRUE == SL_FLAG_GET(CCMR4F_ERROR_FORCING_TEST)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
/** EEPROM Correctable Error */
case ESM_G1ERR_EEPROM_CORRERR:
if (TRUE == SL_FLAG_GET(FEE_ECC_TEST_MODE_1BIT)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/* Retrieve the callback parameters */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (sl_flashWREG->EECORRERRADD);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam2 = (sl_flashWREG->EECORRERRCNT);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam3 = (sl_flashWREG->EECORRERRPOS & 0x000001FFu);
break;
/** EEPROM Uncorrectable Error */
case ESM_G1ERR_EEPROM_UNCORRERR:
if (TRUE == SL_FLAG_GET(FEE_ECC_TEST_MODE_1BIT)) {
cancelCallback = TRUE;
callbackCancelCount++;
}
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (sl_flashWREG->EEUNCERRADD);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam2 = (sl_flashWREG->EESTATUS);
break;
#endif
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_)
/** PSON Compare Error */
case ESM_G1ERR_PSCON_COMPARE_ERR:
/*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
if ((PMM_PRCKEYREG_MKEY_ERRFCG_MODE == sl_pmmREG->PRCKEYREG) && (TRUE == SL_FLAG_GET(PSCON_ERROR_FORCING))) {
cancelCallback = TRUE;
} else {
cancelCallback = FALSE;
}
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (((sl_pmmREG->LPDDCSTAT1 & PMM_PSCON_LPDDCSTAT1_LCMPE) >> 16)
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
| (sl_pmmREG->MPDDCSTAT1 & PMM_PSCON_MPDDCSTAT1_MCMPE));
break;
/** PSON Selftest Error */
case ESM_G1ERR_PSCON_SELTEST_ERR:
/*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
if (TRUE == SL_FLAG_GET(PSCON_SELF_TEST)){
/* Since this is a self test related error, it's always intentionally
* created by kicking off the ST in PRCKEYREG. Selftest API takes
* care of clearing this error nothing needs to be done here */
cancelCallback = TRUE;
callbackCancelCount++;
SL_FLAG_CLEAR(PSCON_SELF_TEST);
}
break;
#endif
/** EFUSE Selftest Error */
case ESM_G1ERR_EFUSE_SELTEST_ERR:
/*efuse selftests have synchronous and asynchronous modes.the efuse esm errors are not blocked by disabling interrupt during selftest*/
if ((TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_STUCK_AT_ZERO))||(TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_ECC))){
/* Since this is a self test related error, it's always intentionally
* created by kicking off the ST in PRCKEYREG. Selftest API takes
* care of clearing this error nothing needs to be done here */
cancelCallback = TRUE;
callbackCancelCount++;
SL_FLAG_CLEAR(EFUSE_SELF_TEST_ECC);
SL_FLAG_CLEAR(EFUSE_SELF_TEST_STUCK_AT_ZERO);
}
break;
/** EFUSE Error */
case ESM_G1ERR_EFUSE_ERR_OTHER:
/*efuse has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
if (TRUE == SL_FLAG_GET(EFUSE_SELF_TEST_ECC)){
/* Since this is a self test related error, it's always intentionally
* created by kicking off the ST in PRCKEYREG. Selftest API takes
* care of clearing this error nothing needs to be done here */
cancelCallback = TRUE;
callbackCancelCount++;
SL_FLAG_CLEAR(EFUSE_SELF_TEST_ECC);
}
break;
#if defined(_TMS570LS31x_) || defined(_TMS570LS12x_) || defined(_TMS570LS07x_) || defined(_TMS570LS09x_) || defined(_RM48x_) || defined(_RM46x_) || defined(_RM44x_) || defined(_RM42x_) || defined(_TMS570LS04x_)
/** PLL2 Slip error **/
case ESM_G1ERR_PLL2_SLIP:
/** Store the callback parameters & reset the status registers */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (uint32)((uint32)(sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u);
break;
/** DCC Error */
case ESM_G1ERR_DCC2_ERR:
callbkParam1 = sl_dccREG2->CNT0;
callbkParam2 = sl_dccREG2->CNT1;
/* Clear Error Flag */
sl_dccREG2->STAT = DCC_DCCSTAT_ERR_FLG;
break;
#endif
#if defined(_TMS570LC43x_) || defined(_RM57Lx_)
/* CCMR5 Self-Test Compare error */
case ESM_G1ERR_CCMR5_SELFTEST:
/*ccmr5f selftests have has synchronous and asynchronous modes,the
* esm errors are not blocked by disabling interrupt during
* selftest*/
/* blocking the esm application call back if the interrupt was due to
* a selftest.
* NOTE: Getting here implies that the CCMR5F has an error! */
if ((TRUE == SL_FLAG_GET(CCMR5F_CPUCOMP_SELF_TEST)) ||
(TRUE == SL_FLAG_GET(CCMR5F_VIMCOMP_SELF_TEST)) ||
(TRUE == SL_FLAG_GET(CCMR5F_PDCOMP_SELF_TEST)) ||
(TRUE == SL_FLAG_GET(CCMR5F_INMCOMP_SELF_TEST))) {
/* clear the ESM Status flag */
BIT_SET(sl_esmREG->SR1[0], BIT(ESM_G1ERR_CCMR5_SELFTEST));
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_CCMR5_OPERATING_STATUS:
callbackCancelCount++;
cancelCallback = TRUE;
sl_esmREG->SR7[0] = GET_ESM_BIT_NUM(ESM_G1ERR_CCMR5_OPERATING_STATUS);
break;
case ESM_G1ERR_DMA_ECC_SBERR:
if(TRUE == SL_FLAG_GET(DMA_ECC_TEST_MODE_1BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_DMA_ECC_UNCORR:
if(TRUE == SL_FLAG_GET(DMA_ECC_TEST_MODE_2BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_CAN1_ECC_SBERR:
case ESM_G1ERR_CAN2_ECC_SBERR:
case ESM_G1ERR_CAN3_ECC_SBERR:
case ESM_G1ERR_CAN4_ECC_SBERR:
if(TRUE == SL_FLAG_GET(CAN_ECC_TEST_MODE_1BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_CAN1_ECC_UNCORR:
case ESM_G1ERR_CAN2_ECC_UNCORR:
case ESM_G1ERR_CAN3_ECC_UNCORR:
case ESM_G1ERR_CAN4_ECC_UNCORR:
if(TRUE == SL_FLAG_GET(CAN_ECC_TEST_MODE_2BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_SPI1_ECC_SBERR:
case ESM_G1ERR_SPI2_ECC_SBERR:
case ESM_G1ERR_SPI3_ECC_SBERR:
case ESM_G1ERR_SPI4_ECC_SBERR:
case ESM_G1ERR_SPI5_ECC_SBERR:
if(TRUE == SL_FLAG_GET(MIBSPI_ECC_TEST_MODE_1BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_SPI1_ECC_UNCORR:
case ESM_G1ERR_SPI2_ECC_UNCORR:
case ESM_G1ERR_SPI3_ECC_UNCORR:
case ESM_G1ERR_SPI4_ECC_UNCORR:
case ESM_G1ERR_SPI5_ECC_UNCORR:
if(TRUE == SL_FLAG_GET(MIBSPI_ECC_TEST_MODE_2BIT)) {
callbackCancelCount++;
cancelCallback = TRUE;
}
break;
case ESM_G1ERR_PSCON_COMPARE_ERR:
/*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
if ((PMM_PRCKEYREG_MKEY_ERRFCG_MODE == sl_pmmREG->PRCKEYREG) && (TRUE == SL_FLAG_GET(PSCON_ERROR_FORCING))) {
cancelCallback = TRUE;
} else {
cancelCallback = FALSE;
}
callbkParam1 = ((sl_pmmREG->LPDDCSTAT1 & PMM_PSCON_LPDDCSTAT1_LCMPE) >> 16);
break;
case ESM_G1ERR_PSCON_SELTEST_ERR:
/*pscon selftests have has synchronous and asynchronous modes,the efuse esm errors are not blocked by disabling interrupt during selftest*/
/*blocking the esm application call back if the interrupt was due to a selftest*/
if (TRUE == SL_FLAG_GET(PSCON_SELF_TEST)){
/* Since this is a self test related error, it's always intentionally
* created by kicking off the ST in PRCKEYREG. Selftest API takes
* care of clearing this error nothing needs to be done here */
cancelCallback = TRUE;
callbackCancelCount++;
SL_FLAG_CLEAR(PSCON_SELF_TEST);
}
break;
/** PLL1 Slip error **/
case ESM_G1ERR_PLL1_SLIP:
/** Store the callback parameters & reset the status registers */
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
callbkParam1 = (uint32)((sl_systemREG1->GBLSTAT & 0x00000300u) >> 8u);
/*SAFETYMCUSW 134 S MR: 12.2 <APPROVED> Comment_4*/
sl_systemREG1->GBLSTAT |= (sl_systemREG1->GBLSTAT & 0x00000300u);
break;
/** PLL2 Slip error **/
case ESM_G1ERR_PLL2_SLIP:
/** No callback parameters - error cause not defined in device TRM */
break;
#endif
default:
/* nothing here - comment to avoid misra-c warning */
break;
}
/* Call application callback only if it's registered & if it's not masked */
/* the MSB of contains information regarding group and LSB contains the esm channel number*/
if ((0u != ESM_AppCallback) && ((boolean)(FALSE) == cancelCallback)) {
(*(ESM_AppCallback))((uint32)(ESM_GRP1_MASK|esmChannel), callbkParam1, callbkParam2, callbkParam3);
}
return;
}
/*Comment_1:
* "Reason - Needed"*/
/*Comment_2:
* "This function will be called by application so not static"*/
/*Comment_3:
* "Reason - used for creation of code section for interrupt handler"*/
/*Comment_4:
* "Reason - FALSE_POSITIVE The rule requires that the expression should be
* guaranteed to have the same value regardless of the order in which the operands within the expression are evaluated.
* This usually means no more than one volatile access occuring in the expression.The recommendation that simple
* assignments should be used is intended to be restricted to simple assignments of the form x = v and not
* "simple assignments" according to the ISO definition. However, the recommendation does not have to be followed
* in order to be compliant with the rule. You should implement the rule (the value should be independent of the
* evaluation order) for compliance purposes and you might choose to issue a warning for non-simple assignments
* or you might choose to ignore them."*/