This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi there,
Fapi_issueProgrammingCommand() 使用Fapi_AutoEccGeneration模式,请问使用Fapi_AutoEccGeneration模式时候参数pu8EccBuffer和u8EccBufferSizeInBytes需要设置吗?
thanks
那么不建议在操作中对flash state machine进行操作,对吗?
我用的uniflash是V4.5.0.2056, 我可以通过read memory看到0xF0400000区间ECC的值,但是export出后来不能完成generate.
首次烧写程序,ECC是通过uniflash自动生成的,后来更新程序是在bootloader程序内使用自动模式Fapi_AutoEccGeneration生成的,我使用的是RM44芯片。
我现在碰到的问题是更新程序后ECC数据不对,导致ESM模块报flash ECC error, 因为这个过程无法debug,uniflash又无法导出ECC数据,所以不能定位ECC错在哪里?请问您有什么建议吗?
非常感谢!