This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好:
我正在使用TMS470MF06607芯片,现要编写此芯片的BootLoader程序,但是发现官网对于此芯片的说明与例程很少,
目前遇到以下几个问题:
1. 官网上有关6607芯片boot说明全都是tms570的,并且样例完全一样,但是两个芯片的flash分别为F021与F035,两种Flash的驱动可以互相替换么?
2. 6607 boot程序中 是否能够打开定时器中断,因为我不止需要CAN bus 的boot 而且也需要在boot程序使用spi接口访问SD卡。实现CAN与SD卡双通道升级。SD卡使用需要有跳出机制,需要有定时器。
并且有哪位工程师有TMS470MF06607 芯片的boot程序可供参考,可以发我邮箱,感谢!