This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash F021库编程TMS570LS0914芯片出错

Other Parts Discussed in Thread: TMS570LS0914

大家好,

我在使用Flash F021库编程TMS570LS0914芯片。

进行了两次写入,第一次成功了,但是第二次失败了。

第一次写入的地址是0x00020000,长度是0x0FFC,也就是写入了4094个bytes。不是4096个bytes。

第二次写入的地址是0x00020FFE,也是写入4094个bytes,然后这一次写入出问题了,显示是写入成功,但是check的时候失败了,并且读内存的时候发现全部都是0xFFFFFFFF,也就是说明没有写入。

想知道问题出在哪里?

1.TMS570LS0914芯片的flash操作是否有单次最小写入长度?4或者是16bytes?

2.TMS570是32位芯片,是否写入的buffer必须是32位长度?

期待您能回答我的问题!谢谢!