Other Parts Discussed in Thread: TMS570LS3137
使用的TMS570LS3137的FEE功能时,遇到了一些问题。
现在的现象是:
1、单独测试读功能 TI_Fee_ReadSync(), 返回值一直为E_OK;
2、单独测试写功能 TI_Fee_WriteSync(), 在连续写817次后,该函数会返回E_NOT_OK,然后读取状态为BUSY,间隔一会在读取状态还是为BUSY;
3、在检测状态为BUSY后,重新初始化FEE,就可以接着进行写操作,但是又是再连续写816次后重复现象2。
初始化参考了HCG中的程序,HCG配置如下图所示:
测试的程序如下:
int main(void)
{
uint16 pos_No = 0;
uint16 read_pos_No = 0;
eepromInit();
while (1)
{
sciPrintf("\n->write %d", pos_No);
eepromWrite(2, (uint8 *)&pos_No);
TI_Fee_ReadSync(2, 0, (uint8 *)&read_pos_No, 2);
sciPrintf("\n->read %d", read_pos_No);
delay_ms(300);
pos_No++;
}
}
uint8 eepromWrite(uint16 block, uint8 *data)
{
Std_ReturnType error = E_OK;
TI_FeeModuleStatusType status;
error = TI_Fee_WriteSync(block, data);
if (error != E_OK)
{
status = TI_Fee_GetStatus(0);
printEEPROMStatus(block, status);
eepromInit();
}
return error;
}
void printEEPROMStatus(uint16 block, TI_FeeModuleStatusType status)
{
switch (status)
{
case UNINIT:
sciPrintf("UNINIT");
break;
case IDLE:
sciPrintf("IDLE");
break;
case BUSY:
sciPrintf("BUSY");
break;
case BUSY_INTERNAL:
sciPrintf("BUSY_INTERNAL");
break;
default:
break;
}
}
希望TI工程师能解答探讨一下,谢谢。