This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms570lc4357 的spi4 操作ais328dq 模块



SPI4 是MIBSPI4 的一种简化模式,配置时使用SPI模式,片选贤使用的是CS[1]、时钟设置的500K,16bit,polarity =1,phase =0;其他值默认。

采用下面的程序读取ais328dq 芯片 设备寄存器WHO_AM_I register 的值(手册上为0x32),但读取的结果 receiveData = 0xFFFF。

 spiInit();

spiDAT1_t dataConfig ={0,0,SPI_FMT_0,SPI_CS_1};

 sendData =0x8f00;
  spiTransmitAndReceiveData(spiREG4, &dataConfig, 1,&sendData, &receiveData);

我想请教上面的程序操作是否对?有没有关于这个模块的使用例子。

  • 您可以尝试参考下面的代码

    • MIBSPI1用于将数据发送到SPI4(必须进行外部连接)
    • MIBSPI1使用DMA将数据从RAM传输到MIBSPI RAM进行传输。
    • SPI4接收DATA,中断用于读取传入的数据并移至RAM
    • SPI4在接收后使用DMA将数据从MIBSPI RAM移至RAM,然后将数据发送至MIBSPI1(也使用中断)

    您可以专注于SPI4代码以查看如何管理中断。

    4331.TMS570LS1224_MIPSPI1_SPI4_DMA.zip

  • 另外也可以参考下面的代码

    /** @file example_SPI_Master_Slave.c
    *   @brief Application main file
    *   @date 25.July.2013
    *   @version 03.06.00
    *
    *   This file contains an example of SPI1 and SPI2 Master / Slave configurations.
    *
    *   PIN Connections must be as Below
    *     ---------------         ---------------
    *     SPI1 ( Master )          SPI2 ( SLave)
    *     ---------------         ---------------
    *     SIM0             --->    SIMO
    *     S0MI             <---    SOMI
    *     CLK              --->    CLK
    *     CS0              --->    CS0
    *
    *  ------------------
    *  GUI configurations
    *  ------------------
    *  1) Driver TAB
    *       - Select SPI2
    *       - Select SPI1
    *  2) VIm Channel 0-31
    *       - Enable SPI2 Level 0 and Level 1 channels.
    *  3) SPI2 TAB
    *       - SPI2 Global SubTAB
    *       	- Uncheck Master Mode
    *       	- Uncheck Internal Clock
    *       - SPI2 Port SubTAB
    *       	- Uncheck DIR for CS 0
    *  3) SPI1 TAB
    *       - Have it default
    *  4) Generate Code.
    *
    */
    
    /* (c) Texas Instruments 2009-2013, All rights reserved. */
    
    /* 
    * Copyright (C) 2009-2015 Texas Instruments Incorporated - www.ti.com
    * 
    * 
    *  Redistribution and use in source and binary forms, with or without 
    *  modification, are permitted provided that the following conditions 
    *  are met:
    *
    *    Redistributions of source code must retain the above copyright 
    *    notice, this list of conditions and the following disclaimer.
    *
    *    Redistributions in binary form must reproduce the above copyright
    *    notice, this list of conditions and the following disclaimer in the 
    *    documentation and/or other materials provided with the   
    *    distribution.
    *
    *    Neither the name of Texas Instruments Incorporated nor the names of
    *    its contributors may be used to endorse or promote products derived
    *    from this software without specific prior written permission.
    *
    *  THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS 
    *  "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT 
    *  LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    *  A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT 
    *  OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, 
    *  SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES INCLUDING, BUT NOT 
    *  LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    *  DATA, OR PROFITS; OR BUSINESS INTERRUPTION HOWEVER CAUSED AND ON ANY
    *  THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT 
    *  INCLUDING NEGLIGENCE OR OTHERWISE ARISING IN ANY WAY OUT OF THE USE 
    *  OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    */
    
    /* USER CODE BEGIN (0) */
    /* USER CODE END */
    
    /* Include Files */
    
    #include "sys_common.h"
    #include "system.h"
    
    /* USER CODE BEGIN (1) */
    #include "spi.h"
    /* USER CODE END */
    
    /** @fn void main(void)
    *   @brief Application main function
    *   @note This function is empty by default.
    *
    *   This function is called after startup.
    *   The user can use this function to implement the application.
    */
    
    /* USER CODE BEGIN (2) */
    uint16 TX_Data_Master[16] = { 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07, 0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F, 0x10 };
    uint16 TX_Data_Slave[16]  = { 0x11, 0x12, 0x13, 0x14, 0x15, 0x16, 0x17, 0x18, 0x19, 0x1A, 0x1B, 0x1C, 0x1D, 0x1E, 0x1F, 0x20 };
    uint16 RX_Data_Master[16] = { 0 };
    uint16 RX_Data_Slave[16]  = { 0 };
    /* USER CODE END */
    
    void main(void)
    {
    /* USER CODE BEGIN (3) */
    
    	spiDAT1_t dataconfig1_t;
    
    	dataconfig1_t.CS_HOLD = FALSE;
    	dataconfig1_t.WDEL    = TRUE;
    	dataconfig1_t.DFSEL   = SPI_FMT_0;
    	dataconfig1_t.CSNR    = 0xFE;
    
    
    	/* Enable CPU Interrupt through CPSR */
    	_enable_IRQ();
    
    	/* Initialize SPI Module Based on GUI configuration
    	 * SPI1 - Master ( SIMO, SOMI, CLK, CS0 )
    	 * SPI2 - Slave  ( SIMO, SOMI, CLK, CS0 )
    	 * */
    	spiInit();
    
    	/* Initiate SPI2 Transmit and Receive through Interrupt Mode */
    	spiSendAndGetData(spiREG2, &dataconfig1_t, 16, TX_Data_Slave, RX_Data_Slave);
    
    	/* Initiate SPI1 Transmit and Receive through Polling Mode*/
    	spiTransmitAndReceiveData(spiREG1, &dataconfig1_t, 16, TX_Data_Master, RX_Data_Master);
    
    	while(1);
    /* USER CODE END */
    }
    
    /* USER CODE BEGIN (4) */
    /* USER CODE END */