1.关于TMS570LS31xHDK的开发板,光盘中为什么没有关于开发板原理图的资料介绍呢?该去哪里找到这些资料呢?
2.在用CCSv5.1进行写入时,总是出错,内容是:Load program Error File:E:\TMS570LS31x_demo_software.out:a date verification error occurred,file load failed.这是为什么呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.关于TMS570LS31xHDK的开发板,光盘中为什么没有关于开发板原理图的资料介绍呢?该去哪里找到这些资料呢?
2.在用CCSv5.1进行写入时,总是出错,内容是:Load program Error File:E:\TMS570LS31x_demo_software.out:a date verification error occurred,file load failed.这是为什么呢?
Hi Bill,
请至下面的地址下载:
http://software-dl.ti.com/dsps/forms/self_cert_export.html?prod_no=ccs_setup_5.3.0.00090.exe&ref_url=http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv5/CCS_5_3_0/
现在我在使用TMS570开发板,但是不知什么原因导致现在无法往板子里面下载程序(昨天的时候还是可以的),用Code Composer Studio v5.1进行RUN——Debug运行后,Code Composer Studio v5.1直接关闭了;用nowFlash往里面Execute光盘内自带的Demo.out文件,也只在进程页面上显示5行指令就结束;用Hercules Safety MCU Demos 自动往里面下载,也是显示(nowFlash has encountered an error while programming the device. Please ensure that the device is correctly connected and then try running the demo again.) 。
不知是什么原因导致了板子无法下载程序?各位有遇到这种的情况吗?
Bill,
您好,TMS570LS31x 系列产品是基于ARM的Cortex-R4F内核,关于ARM的产品分类您可以到一下网址仔细了解下:
http://www.arm.com/products/index.php
如有问题,我们再交流,谢谢!