Other Parts Discussed in Thread: TMS570LS0432
如图所示,通过TTL-232R-5V连接线将PC与EVM1402连接,无法打开COM端口。(windows系统)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TMS570LS0432
如图所示,通过TTL-232R-5V连接线将PC与EVM1402连接,无法打开COM端口。(windows系统)
请确保您对EVM中的SW2设置正确。
请确保笔记本电脑可以在“设备管理器”中正确识别设备。
有时,在控制面板设备管理器中将COM端口更改为其他数字也可以解决此问题,以防发生冲突。

https://www.ti.com.cn/cn/lit/ug/spnu612a/spnu612a.pdf
您可以找一下TMS570LS04x/03x LaunchPad 评估套件开发板上的 R8/R9
另外之前帖子提到的客户问题,最后检查是连接松动了
我没有找到EVM中的SW2,SW2具体在EVM的哪个地方?我用的板子是EVM1402EVM-580,这个上面根本没有SW2!
我按照文档的连接方式连接了,但是bq76PL455_GUI软件还是无法打开com端口。
是不是必须确保电池组连接正确,bq76PL455_GUI软件才可以正常使用?
如果我不接12V电源和16节电池组,bq76PL455_GUI软件是否会正常打开com端口?
目前的流程就是如user6365912所示的那样。关于使用的资料,就只有我之前提供的文档。
另外我在E2E也找了相关专家询问,您可以补充一下您现在的信息