您好,在2 级和3 级(L2 和L3)互连子系统中,提到“基本功能性的软件测试”,强烈建议使用基本功能性的引导时间软件测试,我查看Cortex-R4的手册,貌似没有L3系统啊,请问“基本功能性的引导时间软件测试”是怎么实现的呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,在2 级和3 级(L2 和L3)互连子系统中,提到“基本功能性的软件测试”,强烈建议使用基本功能性的引导时间软件测试,我查看Cortex-R4的手册,貌似没有L3系统啊,请问“基本功能性的引导时间软件测试”是怎么实现的呢?
Hi Wei,
你说的应该是安全手册的5.11.6中的内容吧?
这段的英文原文如下:
5.11.6 Software Test of Basic Functionality Including Error Tests
A software test can be utilized to test for basic functionality as well as to inject diagnostic errors and check
for proper error response. Such a test can be executed at boot or periodically. Software requirements
necessary are defined by the software implemented by the system integrator. The use of a boot time
software test of basic functionality is highly recommended. The use of a periodic software test of basic
functionality reporting is recommended.
这里说的L2和L3是指MCU内部的系统,一般被成为Subsystem,这个Sub是跟CPU相对应的。
5.11开篇有这样的描述:
The system interconnect is composed of a number of bridges, gaskets, communications crossbars, and
routing logic, which connects the bus masters (DMA, CPU, TUs, and so forth) to L2 slaves and L3
peripherals.
一般来说,用户不用特别关心和理解L2和L3的区别,但是需要知道在MCU构架下,外设是如何与CPU建立连接的。
了解了这个架构,就能更好的预估哪里有可能出问题,从而设计系统来规避或不断检测是否有问题存在。
所以L2,L3应该是MCU的概念,而不是CPU的概念,ARM的手册应该不会提及。
“基本功能性的引导时间软件测试”..........
我觉得还是建议中英文对照来看文档,这句在英文原文里是"The use of a boot time software test of basic functionality is highly recommended."
即"我们非常建议用户在系统启动时,对基本功能进行软件测试。"