你好,除了eclk管脚外,其他的管脚没有pll功能么,我需要的频率是大于20MHz的,CPU的PLL不能输出个更高频率的时钟么?不能使用CPU提供一个更高频率的时钟么?如果可以怎么设计
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,除了eclk管脚外,其他的管脚没有pll功能么,我需要的频率是大于20MHz的,CPU的PLL不能输出个更高频率的时钟么?不能使用CPU提供一个更高频率的时钟么?如果可以怎么设计
Hi meng,
所有输出的IO只有有IO Buffer存在的都不可能突破IO Buffer的最大速率,即20MHz。
如果你需要20MHz,可以尝试使用HET来输出一个高速PWM。
在180MHz的时钟频率下,设置VCLK2=180MHz,HR=1,LR=4,然后写两条HET指令为产生一个高速PWM,频率可以达到22.5MHz。但是,这样的将使你无法再使用HET模块做其他事情,因为HR=1, LR=4的设置,只允许跑4个周期的HET指令。
综合考虑,还是建议配一个外置晶振。
Regards,
Jay