Other Parts Discussed in Thread: HALCOGEN
1、使用串口的isp下载程序,程序代码应该从0X00020000开始,如何设置;
2、是否可支持程序在RAM中运行(觉得应该可以),如何设置,是否比FLASH中快,以前了解过DSP可以将FLASH的代码COPY到RAM中运行,这一条只是了解一下,实际可能不会用到,3137是否像STM的ARM-M3那样支持直接在RAM中运行程序,这样特别是开发板可以减少FLASH的使用频率,增加寿命。
3、从VIM章节了解到3137应该是不支持中断向量重定向的,但是在工程生成的.map文件中从0开始有20H字节的VECTORS是什么??
4、3137 reference Manual中de VIM 寄存器章节 offset 地址没有顺序往下排,在HAL生成的VimBase的定义中比如FIRQPR3应该是个reserved,不是只有96个中断吗,怎么会有4个32位的寄存器呢(HAL生成的代码是否不够严谨)