This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137 USB评估板 VCLK1问题

Other Parts Discussed in Thread: HALCOGEN

CCS5.4.0.00091 ,HALCOGEN03.02.02,在做评估板实验时,只选择SCI2驱动,设置GCM中VCLK1为80Hz时,串口设置参数115200,2停止位,8数据,没有使用中断发送,串口可以正常工作。当设置GCM中VCLK1为160MHz时,其余参数不变化,下载后程序无法跳到main,在自检程序 hetParityCheck(有时htu1ParityCheck)中死循环或者在dabort.asm中,请问下,如果我要想使用400K以上的波特率时,还需怎么设置?谢谢