Other Parts Discussed in Thread: TMS570LS3137, TMS570LS1114
TMS570LS31x/21x TRM(SPNU499B)的IOMM一节的表4-1中的最后一项GIOB[2],它的dedicated input pin为142,
但是在数据表上142引脚为FRAYTXEN1,没有提到GIO的功能,是否手册有误?表上的Control Register bit A 和B都是
PINMMR29[16],无法套用下面的选择规则
The input to a module comes from the multiplexed pin when the condition [ A and not(B) ] = TRUE.
• The input to a module comes from the dedicated pad when the condition [ not(A) or (A and B) ] =TRUE.
请问如何配置这个端口。