This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570与RM48X



问下TMS570与RM48X的主要区别有哪些?

  • Hi ZhiQiang,

      TMS570和RM48X都是我们Hercules安全MCU中的两个系列。他们的主要区别分为以下几个方面:

    1. 在安全标准的认证方面,我们的TMS570通过了IEC61508 SIL-3和ISO26262的 AIL-D的安全标准关于processor具体要求的认证;而RM48X则只通过了IEC61508 SIL-3的认证。换句话说,TMS570更适用于汽车行业,而RM48X则适用于工业和医疗行业

    2. 外设方面:TMS570由于是定位在汽车行业,它本身有几款系列是带有flexray高速总线的,而RM48X则具有USB外设,更好的适用于工业的需求。

    3. 在性能方面,RM48X和TMS570都是cortex-R4F的内核,但是他们支持的运行的最高频率不一样,TMS570为160MHZ(QFP)和180Mhz(BGA),而RM48X则为200Mhz(QFP)和220MHZ(BGA).

    4.在存储方式上面,它们两有不同,TMS570是大端存储模式,RM48X是小段存储模式。这个对于要移植实时操作系统来说比较重要。

    谢谢!

    Ken