This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

问一个SPI的问题

TMS470M中 SPI1并没有相关的ENA引脚 但是SPI2能找到 想问下SPI1不需要外接么?

  • Klapset,

      看上去,应该是MIBSPI1硬件上没有支持这个功能,所以没有硬件的管脚MIBSPIENA。如果你要用这个功能的话,其实你也可以自己定义一个GPIO来连接两个SPI。主设备作为GPIO中断输入用,从设备端作为GPIO输出设置用。当从设备有数据需要发送是,拉低或拉高这个信号,触发主设备中断,然后发送时钟信号给从设备,从而得到相关的数据。这就相当于从设备控制数据流的方向了。

    谢谢