This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在safety manual中,对于各个诊断机制,均有特定的推荐等级,如强制要求,强烈推荐以及可选等,当然这只是TI的建议,用户可以根据实际应用去选择不同诊断机制。如果要符合SIL3等级,需要看具体的安全标准中对于各个指标的要求了,在FMEDA中选择安全机制后,去看一下计算的结果是否满足指标要求,如果不满足要求,可能需要增加安全措施了。另外在安全标准中也会有一些要求,这些也是需要去满足的。
谢谢!
您好!在FMEDA文件中有关于各个模块的失效率计算结果,当在前边设定完用户可以设置的应用环境以及诊断机制后,FMEDA就可以计算出对应的诊断覆盖率等结果了。在SAR2(Detailed safety analysis report)中有关于FMEDA文件的使用说明和例子说明,请参考。
谢谢!
谢谢! 看到了 “Custom diagnostics”这个文件,“this excel sheet allows for applying customer specific safety mechanisms (at the sub module level) not listed in the safety manual”,这个表格是at the sub module level 数据,有没有at the module level 数据呢 ? 我看到Details-IEC61508 是at the module level 数据,却没看到诊断覆盖率DC。请问SAR2在哪个文件中(文件中有很多表格)? 不胜感激!!!!!!!
您好!SAR2就是Detailed safety analysis report文件,at the module level 的数据在FMEDA文件中是在Summary-IEC61508这个表单中显示的。关于DC的问题,在FMEDA文件中的中间几个表格是有计算的,这与采用的安全机制以及客户自己设计的附加安全机制都有关。
另外,这些问题其实涉及到了关于安全标准中非常深入的问题,我建议您去E2E private forum上提问,那里有很多安全方面的专家可以解决您的疑问,并且他们也有很多年和认证公司合作的经验,会给您非常专业的回复。关于E2E private forum的登陆用户名和密码,在签署完NDA协议后TI应该会发给在文件上签字的负责人。
谢谢!