This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

就控制芯片而言,搭建ASIL C等级的硬件平台,使用一个570的芯片就能满足了吗,是否还需要额外的从芯片。

如题,请有相关经验的专家帮忙答复,非常感谢!

  • 您好,TMS570系列MCU可以满足ISO26262 ASIL D等级的要求,如果需要实现ASIL C等级要求,就控制芯片层面而言,使用一颗安全MCU就没有问题了(当然,软件的开发流程和编写也是需要满足安全标准的要求的);为了设计更可靠的系统,一般我们推荐客户搭配TI提供的电源管理芯片TPS65381一起使用,这颗芯片也是经过了安全认证的,这样设计的系统无论在电源还是处理器上都比较有保证。当然,采用分立的电源供电方案也是可以的,只不过用户需要再针对电源部分来设计一些诊断和保护机制。

    谢谢!

  • 回答的很专业,我们现在打算使用570做我们的主控芯片,后期有问题还请多多支持,非常感谢!

  • 您好!谢谢您选择TI的安全MCU来设计产品,为了便于我们更好的支持,我想大致了解一下您目前的项目情况,方便的话能否在邮件中沟通一下,我的邮箱是jason-zhang@ti.com,谢谢!