Other Parts Discussed in Thread: HALCOGEN
本人是新手,在哈里halcogen里面没有找到GIO和I/O block的选项,也不知道在halcogen里面如何操作,才能把4个can引脚设置成i/o,我板子都做好了,一定要设置成i/o口,懂的兄弟帮帮我,谢谢了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!我查了一下,不知道什么原因,在HALCoGen中CAN模块没有CAN Port选项卡,而在其它模块如SPI/SCI中是有这个选项的,在这个选项卡中可以设置引脚是作为功能引脚使用还是作为GPIO来使用。由于没有这个选项,因此可能需要您在HALCoGen生成的代码中人工的去修改一下寄存器的值,从技术手册中可以找到相关的寄存器为CAN TX IO Control Register (DCAN TIOC)以及CAN RX IO Control Register (DCAN RIOC);对于引脚的具体操作也是在这个寄存器中的。
谢谢!