This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570外部时钟晶振问题

Other Parts Discussed in Thread: TMS570LS3137

您好:

        我们公司准备使用TMS570这款芯片来开发产品,关于TMS570我有几个疑问,希望您能帮我解答一下

        我用的芯片型号:TMS570LS3137CPGEQQ1

        我们的产品需要160MHz的频率

        现在我们用的16M的外部晶振是可以正常工作的,在后面的产品中也许会改变晶振频率,我有如下问题

        1、你们的TMS570开发板上选用的是16M的外部晶振,为什么选16M的而不选其他频率的?

        2、如果用8M的晶振是否也可以?和16M的比,对板子的稳定性是否有影响?

        3、如果选择更大的晶振呢,25M、40M的是否也可以?稳定性如何

        4、40M以上的呢?最大可以选择多大的晶振?你们推荐的晶振是多大的?

        谢谢!