This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tms570有没有类似stm32中fsmc的功能呢?

Other Parts Discussed in Thread: TMS570LS0432, CONTROLSUITE

想了解下TI的微控制器芯片中有没有类似以前单片机总线扩展的功能,像STM32中有fsmc功能,可以用地址、数据总线及相应的读、写控制信号线实现扩展功能,不知道hercules系列中会有这种功能吗,或者哪些TI的其他芯片有这些功能

目前需要做一些大量的I/O处理,需要can总线控制器,还有就是得扩展下芯片本身的IO,但是对芯片本身的处理能力又没有太大的要求(最低端的处理速度已经能够满足要求),不清楚您这里对于芯片的选型方面能不能给一些参考建议呢,十分感激

yong zhang

  • yong,

      Hercules里面有EMIF总线接口,可以做一些扩展存储空间的操作。

    对于你的需求,首先看有没有安全方面的需求,如果有的话,建议看下570系列,如果没有的话,可以建议看下我们的TM4C123X系列或是我们的C2000的低端系列的产品。

    谢谢

  • 十分感谢您的回复,我看了下570系列的芯片,TMS570LS0432/0332这两款芯片想了解下IO复用的问题,产品说明中说这两款都有45个I/O引脚,那么如果我做设计的话JTAG调试接口需要占用4个IO?can总线也需要2个IO,那么在实际使用中能够给我操作的IO就只有39个了?是这样计算吗,另外,如果选择c2000系列的芯片的话有没有官方的电路原理图作参考呢?

    yong zhang

  • yong,

      GPIO基本是按这样算的。 你可以考虑用下TM4C123X的产品,它的GPIO应该能满足你的需求。

    对于C2000的产品,你可以到我们的官方上面下载controlsuite,他里面包含了所有的开发板, 程序和相关的文档。

    谢谢

  • 十分感谢您的回答~谢谢了~