Other Parts Discussed in Thread: HALCOGEN
各位TI的专家,
大家好,我需要将FLASH未被烧写的地址对应的ECC也烧入Flash,该怎么办?
我的link文件如下:
/*----------------------------------------------------------------------------*/
/* sys_link.cmd */
/* */
/* (c) Texas Instruments 2009-2013, All rights reserved. */
/* */
/*----------------------------------------------------------------------------*/
/* USER CODE BEGIN (0) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Linker Settings */
--retain="*(.intvecs)"
/* USER CODE BEGIN (1) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Memory Map */
MEMORY
{
/* Flash Memory */
/* Bank 0 */
VECTORS (X) : origin=0x00000000 length=0x00000020 fill=0xffffffff
FLASH0 (RX) : origin=(end(VECTORS)) length=(0x00180000 - size(VECTORS) - 512) vfill=0xffffffff
/* Bank 1 */
FLASH1 (RX) : origin=0x00180000 length=0x00180000 vfill=0xffffffff
/* Bank 0 ECC */
ECC_VEC (R) : origin=(0xf0400000 + (start(VECTORS) >> 3)) length=(size(VECTORS) >> 3) ECC={algorithm=algoR4F021, input_range=VECTORS}
ECC_FLA0 (R) : origin=(0xf0400000 + (start(FLASH0) >> 3)) length=(size(FLASH0) >> 3) ECC={algorithm=algoR4F021, input_range=FLASH0 }
/* Bank 1 ECC */
ECC_FLA1 (R) : origin=(0xf0400000 + (start(FLASH1) >> 3)) length=(size(FLASH1) >> 3) ECC= {algorithm=algoR4F021, input_range=FLASH1 }
STACKS (RW) : origin=0x08000000 length=0x00001500
RAM (RW) : origin=0x08001500 length=0x0003EB00
/* USER CODE BEGIN (2) */
/* USER CODE END */
}
/* USER CODE BEGIN (3) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Section Configuration */
SECTIONS
{
.intvecs : {} > VECTORS
.text : {} > FLASH0 | FLASH1
.const : {} > FLASH0 | FLASH1
.cinit : {} > FLASH0 | FLASH1
.pinit : {} > FLASH0 | FLASH1
.bss : {} > RAM
.data : {} > RAM
.sysmem : {} > RAM
/* USER CODE BEGIN (4) */
/* USER CODE END */
}
/* USER CODE BEGIN (5) */
/* USER CODE END */
/*----------------------------------------------------------------------------*/
/* Misc */
ECC {
algoR4F021 : address_mask = 0x003ffff8 /* Address Bits 21:3 */
hamming_mask = R4 /* Use R4 build in Mask */
parity_mask = 0x0c /* Set which ECC bits are Even and Odd parity */
mirroring = F021 /* RM4x are build in F021 */
}
/*----------------------------------------------------------------------------*/
/*----------------------------------------------------------------------------*/
上面的link文件配置也不能写入FLASH未被烧写的地址对应的ECC????