This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570有哪些程序的加密方式?

TMS570有哪些程序的加密方式?除了烧断熔丝这种普通的方式,还有没有加密性更好的方式?另外TMS470料怎么那么少,是不是要停产的节奏?

  • 自从有了570,用470的人就少了,楼主也可以大胆投靠570怀抱了。烧断熔丝这方法已经很不错了, 实际上没有百分百的保险方法。

  • 首先470是470,570是570,两个定位不同产品。应用场合也不一样,现在有低端的570可以cover 470的应用,而且有过ISO26262 和IEC61508的论证。

    TMS570的加密模式,有以后脚AJSM的模式,你可以查看一下我们的数据手册,或是在论坛里面搜索一下,我们有过这方面的帖子介绍。,

    谢谢