TMS570LC43x开发套件的SCI3当作UART使用时,不能发送数据,为什么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
tms570lc43xx HDK sic如下配置 ,波特率是多少?串口工具接收到数据乱码?
/** - bring SCI1 out of reset */
sciREG1->GCR0 = 0U;
sciREG1->GCR0 = 1U;
/** - Disable all interrupts */
sciREG1->CLEARINT = 0xFFFFFFFFU;
sciREG1->CLEARINTLVL = 0xFFFFFFFFU;
/** - global control 1 */
sciREG1->GCR1 = (uint32)((uint32)1U << 25U) /* enable transmit */
| (uint32)((uint32)1U << 24U) /* enable receive */
| (uint32)((uint32)1U << 5U) /* internal clock (device has no clock pin) */
| (uint32)((uint32)(1U-1U) << 4U) /* number of stop bits */
| (uint32)((uint32)0U << 3U) /* even parity, otherwise odd */
| (uint32)((uint32)0U << 2U) /* enable parity */
| (uint32)((uint32)1U << 1U); /* asynchronous timing mode */
/** - set baudrate */
sciREG1->BRS = 259U; /* baudrate */
/** - transmission length */
sciREG1->FORMAT = 8U - 1U; /* length */
/** - set SCI1 pins functional mode */
sciREG1->PIO0 = (uint32)((uint32)1U << 2U) /* tx pin */
| (uint32)((uint32)1U << 1U); /* rx pin */
/** - set SCI1 pins default output value */
sciREG1->PIO3 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI1 pins output direction */
sciREG1->PIO1 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI1 pins open drain enable */
sciREG1->PIO6 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI1 pins pullup/pulldown enable */
sciREG1->PIO7 = (uint32)((uint32)0U << 2U) /* tx pin */
| (uint32)((uint32)0U << 1U); /* rx pin */
/** - set SCI1 pins pullup/pulldown select */
sciREG1->PIO8 = (uint32)((uint32)1U << 2U) /* tx pin */
| (uint32)((uint32)1U << 1U); /* rx pin */
/** - set interrupt level */
sciREG1->SETINTLVL = (uint32)((uint32)0U << 26U) /* Framing error */
| (uint32)((uint32)0U << 25U) /* Overrun error */
| (uint32)((uint32)0U << 24U) /* Parity error */
| (uint32)((uint32)0U << 9U) /* Receive */
| (uint32)((uint32)0U << 8U) /* Transmit */
| (uint32)((uint32)0U << 1U) /* Wakeup */
| (uint32)((uint32)0U << 0U); /* Break detect */
/** - set interrupt enable */
sciREG1->SETINT = (uint32)((uint32)0U << 26U) /* Framing error */
| (uint32)((uint32)0U << 25U) /* Overrun error */
| (uint32)((uint32)0U << 24U) /* Parity error */
| (uint32)((uint32)1U << 9U) /* Receive */
| (uint32)((uint32)0U << 1U) /* Wakeup */
| (uint32)((uint32)0U << 0U); /* Break detect */
/** - initialize global transfer variables */
g_sciTransfer_t[0U].mode = (uint32)0U << 8U;
g_sciTransfer_t[0U].tx_length = 0U;
g_sciTransfer_t[0U].rx_length = 0U;
/** - Finaly start SCI1 */
sciREG1->GCR1 |= 0x80U;
VCLK = 80 Mhz baudrate = 19200 我计算错了,嘻嘻