最近调试TMS570 SPI接口,使用标准SPI 主从模式通信,SPI4~SPI5互相发送数据。
硬件环境:570板子按要求连接SPI4和SPI5的4个管脚。
驱动配置:配置好主从模式后,生成驱动。
main函数中,主机调用查询模式发送数据,发现发送一个字节数据后,进入WHILE等待接收数据不能退出,造成主机无法发送剩下字节内容!
从机没有任何中断产生。
1、不知道是从机的驱动配置没有配对,还是其他原因。
2、另外,可否有SLAVE的正确配置文档和实例demo,请多多分享下,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.