This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这里的是初始化的程序,请指点是哪里出现的问题,我采样不出来 void adc_init() { P6SEL |=BIT2; // Enable A/D channel A0 ADC12CTL0 = ADC12ON+ADC12SHT0_8+ADC12MSC; // Turn on ADC12, set sampling time // set multiple sample conversion ADC12MCTL2=ADC12INCH_2; ADC12CTL1 = ADC12SHP+ADC12CONSEQ_2; // Use sampling timer, set mode ADC12IE = 0x04; // Enable ADC12IFG.2 ADC12CTL0 |= ADC12ENC; // Enable conversions ADC12CTL0 |= ADC12SC; // Start conversion __bis_SR_register(GIE); } 中断向量10里面读出ADC12MEM2 case 10:results= ADC12MEM2; 程序一直不能正常运行,请问哪里出现了问题?谢谢指教! |
问题已找到,中断位置不对,我的单片机也有问题,在别人的板子上修改一下中断入口就可以运行了,TI给学校的5529板子,我的是有点问题的,我之前用ADC的时候一直配置P6.1(我也不知道当时怎么想的)但是我接在P6.0上一直可以用,但是有一次测量的时候,P6.0口烧毁了,这时候才发现我之前配置的程序是有问题的,现在同样的程序,在别人的单片机上是可以运行的,在我的上面就不能运行,希望遇到同样问题的朋友要敢于怀疑他们的板子,真的是有问题的!!!我的板子来的时候就有IO口直接接在地上的,tft驱动搞了好久才发现有两个IO不受控制一直是低电平,弄了很久才发现这样的错误!建议拿到板子先看看有没有IO直接对地短接!