This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS编程时 出现这样的警告提示 "Twidd_256" overflowed; the 17-bit relocated address 0x10546 is too large to encode in the 16-bit field

哪位大神可以告诉我一下呀 谢谢  "Twidd_256" overflowed; the 17-bit relocated address 0x10546 is too large to encode in the 16-bit field    大体意思我知道 我想知道怎么改我的代码 或者怎么将更改数组地址  谢谢