This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 6.1.2 中的三种警告应该怎么处理。



我是在ti官网上下载的  例程,   添加项目后 编译 出现三种警告, 应该怎么处理呢。用的是CCS 6.1.2 的编译器

1、Description Resource Path Location Type,#163-D unrecognized #pragma hal_mcu.c /CC85xx_EHIF_lib line 43 C/C++ Problem。    

2、Description Resource Path Location Type.

This project was created using a version of compiler that is not currently installed: 4.2.3 [MSP430]. Another version of the compiler will be used during build: 4.4.5. Please go to <a href="liveaction:OpenAppCenter">CCS App Center</a> to install the compiler of the required version, or migrate the project to one of the available compiler versions by adjusting project properties. CC85xx_EHIF_lib properties Problems

3、section WP_master.out(.const) was padded by 1 to a size of 166 to.

这三种警告应该怎么解决呢。