This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我目前正用MSP430FG6426做一个项目,同时应用了XT1和XT2作为时钟源:
XT1 32.768KHZ
XT2 20MHZ
但是XT1一直不能工作,在这个MCU中XT1的PIN脚,是独立的不需要另外的设置。
我们的硬件工程师已经检查过电路了,但是XT1就是不起振,X2却工作正常。在我们另外的一个项目中应用MSP430F5系列时,XT1也不起振。
因为两款芯片都是XT1是独立IO的,没有另外的寄存器可以配置。
还请TI的工程师帮忙看看,如果你们有应用成功的例子,也可以告诉我。