问题描述:
1. MSP430F5509+CC1101在实现定时发送无线数据包的功能时,偶尔会产生XT1 fault。
2. 取100个设备进行测试,在运行一段时间后,大约会有7个设备产生了XT1 fault。
3. 使用数字电源,串联30欧姆电阻,为设备供电,每一个设备都会产生XT1 fault。
4. XT1 fault产生的时间,是在CC1101发送数据包完成后的瞬间,接收端可以收到此数据包。
5. 将程序中的所有的__bis_SR_register(LPM3_bits + GIE);更改为__bis_SR_register(LPM0_bits + GIE);,仍然会出现XT1 fault。
6. 去除程序中所有的__bis_SR_register(LPM3_bits + GIE);,稍作修改,使得程序可以实现预定功能,未出现XT1 fault。
注:
1. MCLK = DCODIV = 12MHz, SMCLK = DCODIV = 12MHz, ACLK = XT1 = 32.768KHz, FLL reference = XT1CLK
2. CC1101发送数据包时,设备的总电流大约40mA,耗时10ms。
3. XT1 = 32.768KHz外部晶振, -20 < PPM < 20, LF mode
求助:
1. 什么情况下可以产生XT1 fault ?
2. 产生XT1 fault后,需要进行哪些操作,使得系统可以尽快回到正常工作状态?
UCS的设置函数:
/******************************************************************************* * @fn: InitSysClk_12MHz * @brief: MCLK = SMCLK = DCOCLKDIV = 12MHz, ACLK = XT1CLK = 32.768KHz * @para: none * @return: * 0 = ok * -1 = XT1 error * -2 = DCO error * -3 = XT1 error && DCO error * -4 = XT2 error * -5 = XT1 error && XT2 error * -6 = DCO error && XT2 error * -7 = XT1 error && DCO error && XT2 error ******************************************************************************/ signed char InitSysClk_12MHz(void) { signed char rc = 0; *Address = 0x9628; *(Address + 4) = 0x0800; *Address = 0x9600; P1SEL |= BIT0; P1DIR |= BIT0; P5SEL |= BIT4 | BIT5; // Select XT1 UCSCTL6 &= ~(XT1OFF); // XT1 On UCSCTL6 |= XCAP_3; // Internal load cap UCSCTL3 = 0; // FLL Reference Clock = XT1 // Loop until XT1,XT2 & DCO stabilizes - In this case loop until XT1 and DCo // settle unsigned int delay = 60000; do { UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags if (--delay == 0) { if (UCSCTL7 & XT1LFOFFG) { // XT1 error rc += -1; } if (UCSCTL7 & DCOFFG) { // DCO error rc += -2; } if (UCSCTL7 & XT2OFFG) { // XT2 error rc += -4; } return rc; } } while (SFRIFG1 & OFIFG); // Test oscillator fault flag UCSCTL6 &= ~(XT1DRIVE_3); // Xtal is now stable, reduce drive strength UCSCTL4 |= SELA_0; // ACLK = LFTX1 (by default) UCSCTL3 = SELREF_0; // Set DCO FLL reference = REFO UCSCTL0 = DCO0 | 0x0000; // Set lowest possible DCOx, MODx __bis_SR_register(SCG0); // Disable the FLL control loop UCSCTL1 = DCORSEL_5; // Select DCO range 16MHz operation UCSCTL2 = FLLD_0 + 365; // Set DCO Multiplier for 8MHz // (N + 1) * FLLRef = Fdco // (365 + 1) * 32768 = 12MHz __bic_SR_register(SCG0); // Enable the FLL control loop // Worst-case settling time for the DCO when the DCO range bits have been // changed is n x 32 x 32 x f_MCLK / f_FLL_reference. See UCS chapter in 5xx // UG for optimization. // 32 x 32 x 12 MHz / 32,768 Hz = 375000 = MCLK cycles for DCO to settle __delay_cycles(375000); // Loop until XT1,XT2 & DCO fault flag is cleared delay = 60000; do { UCSCTL7 &= ~(XT2OFFG | XT1LFOFFG | DCOFFG); // Clear XT2,XT1,DCO fault flags SFRIFG1 &= ~OFIFG; // Clear fault flags if (--delay == 0) { if (UCSCTL7 & XT1LFOFFG) { // XT1 error rc += -1; } if (UCSCTL7 & DCOFFG) { // DCO error rc += -2; } if (UCSCTL7 & XT2OFFG) { // XT2 error rc += -4; } return rc; } } while (SFRIFG1 & OFIFG); // Test oscillator fault flag PMMCTL0_H = PMMPW_H; // PMM Password SVSMHCTL &= ~(SVMHE | SVSHE); // Disable High side SVS SVSMLCTL &= ~(SVMLE | SVSLE); // Disable Low side SVS return 0; }