This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430 G2553 Timer_A主定时器外部时钟输入



写了个小的测试程序,使用外部时钟输入,但是总没有计数的效果。输入的信号是信号发生器产生的方波(-3V~3V,频率32768Hz),代码如下:

#include "MSP430G2553.h"
#include "LCD_128.h"
#include "HT1621.h"
#include "TCA6416A.h"


unsigned char flag1=0;
unsigned char flag2=0;
unsigned int temp=0;
long temp1;
long FRE=12346;
long adc_sample=0;
long adc_max=0;
unsigned int i;

void main( void )
{
WDTCTL = WDTPW + WDTHOLD; //关狗

TCA6416A_Init();
HT1621_init();

P1DIR |= BIT6; //使用P1.0控制LED闪烁
P1SEL |= BIT0;
P1DIR &= ~BIT0;


TA1CCTL0=CCIE; //Capture/compare interrupt enable
TA1CCR0=32768; //设置计数周期
TA1CTL= TASSEL_0 + MC_1 +TACLR;//选择时钟源,SMCLK;计数模式,连续计数

while(1)
{
_BIS_SR(LPM0_bits + GIE);
temp1=FRE;

}
}


#pragma vector=TIMER1_A0_VECTOR
__interrupt void Timer1_A (void)
{


// _BIC_SR_IRQ(LPM0_bits);
P1OUT^=BIT6;

}