This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430串口只进行数据接收TXD断开,只进接收中断一次,接收一组数据完成后要关闭并打开串口一次才能进入接收中断进行下一次接收



#include <msp430x16x.h>

unsigned char RecBuf[35]; //接收数据缓存
unsigned char Rindex; //接收数据计数
unsigned char Rinflag; //接收血糖数据包完毕标志
/*******************************************************/
void Uart_init(void);
/*******************************************************/
void Uart_init(void)
{
P3SEL |= 0x30; // 选择P3.4TX和P3.5RX做UART通信端口
ME1 |= UTXE0 + URXE0; // 使能USART0的发送和接受
UCTL0 |= CHAR; // 选择8位字符
UTCTL0 |= SSEL1; // UCLK = SMCLK时钟源选择8M
UBR00 = 0x8A; // 波特率57600设定
UBR10 = 0x00; //
UMCTL0 = 0xDE; // Modulation
UCTL0 &= ~SWRST; // 初始化UART状态机
IE1 |= URXIE0; // 使能USART0的接收发送中断
}
/*******************************************************/
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // 关闭看门狗
volatile unsigned int i;
BCSCTL1 &= ~XT2OFF; // XT2on
do
{
IFG1 &= ~OFIFG; // Clear OSCFault flag
for (i = 0xFF; i > 0; i--); // Time for flag to set
}
while ((IFG1 & OFIFG)); // OSCFault flag still set
BCSCTL2 |= SELM_2 + SELS; // MCLK = SMCLK = XT2 (safe)

Uart_init();

while(1)
{
_BIS_SR(LPM0_bits+GIE);
//IE1 |= URXIE0; // 使能USART0的接收发送中断
}
}

#pragma vector = UART0RX_VECTOR
__interrupt void UART0_RXISR(void)
{
RecBuf[Rindex++] = RXBUF0;
if(RecBuf[Rindex-2]==0xFE) //接收完毕
{
Rindex=0;
if(RecBuf[0]==0x5F) //帧头正确
{
Rinflag=1;
}
}
}