This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: USS Module issue consultation

Part Number: MSP430FR6043

const USS_App_AddlTXSequence_t  addtlTXSeqs[USS_APP_ADDTL_TX_SEQUENCES_MAX] =
{
     // Sequence #1
     // 2 trill pulses
     // X-pulse #1 = 1 @300kHz (with 80Mhz PLL)  @ 571k
     // E-pulse #1 = 1 @400kHz (with 80Mhz PLL)  @ 667k
     // X-pulse #2 = 2 @500kHz (with 80Mhz PLL)  @ 800k
     // E-pulse #2 = 3 @800kHz (with 80Mhz PLL)  @ 1M
     {
         .numTrillCycles = 2,
         .xpulse = { 1, 2 },
         .xhper = { 133, 80 },  // 80Mhz / (133+133) = ~300kHz
         .xlper = { 133, 80 },  // 80Mhz / (80+80) = 500kHz
         .epulse = { 1, 3 },
         .ehper = { 100, 50 },  // 80Mhz / (100+100) = 400kHz
         .elper = { 100, 50 },  // 80Mhz / (50+50) = 800kHz
         .binPatternLen = 25,   // 25 counts of binary pattern at 8Mhz
         .binPattern =
         { 1,1,1,-1,-1,-1,1,1,1,-1,-1,1,1,-1,-1,1,1,-1,-1,1,-1,1,-1,1,-1},
     }
};

 

In the program, what is the relationship between the frequency of the transmitted wave and binPatternLen, binPattern? If the frequency of the transmitted wave is modified, how should the corresponding values of binPatternLen and binPattern be adjusted?