This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5529的开发板怎样向电脑发送数据啊

Other Parts Discussed in Thread: MSP430F5529

MSP430F5529的开发板怎样向电脑发送数据啊,最近一直在搞这个,不知道怎么写的,希望好心人提示一下,谢谢了

  • 如下是一个自发自收的例程,看懂了稍微改一下就行。

    /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //   MSP430F552x Demo - USCI_A0, 115200 UART Echo ISR, DCO SMCLK
    //
    //   Description: Echo a received character, RX ISR used. Normal mode is LPM0.
    //   USCI_A0 RX interrupt triggers TX Echo.
    //   Baud rate divider with 1048576hz = 1048576/115200 = ~9.1 (009h|01h)
    //   ACLK = REFO = ~32768Hz, MCLK = SMCLK = default DCO = 32 x ACLK = 1048576Hz
    //   See User Guide for baud rate divider table
    //
    //                 MSP430F552x
    //             -----------------
    //         /|\|                 |
    //          | |                 |
    //          --|RST              |
    //            |                 |
    //            |     P3.3/UCA0TXD|------------>
    //            |                 | 115200 - 8N1
    //            |     P3.4/UCA0RXD|<------------
    //
    //   Bhargavi Nisarga
    //   Texas Instruments Inc.
    //   April 2009
    //   Built with CCSv4 and IAR Embedded Workbench Version: 4.21
    //******************************************************************************
    
    #include <msp430.h>
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
    
      P3SEL |= BIT3+BIT4;                       // P3.3,4 = USCI_A0 TXD/RXD
      UCA0CTL1 |= UCSWRST;                      // **Put state machine in reset**
      UCA0CTL1 |= UCSSEL_2;                     // SMCLK
      UCA0BR0 = 9;                              // 1MHz 115200 (see User's Guide)
      UCA0BR1 = 0;                              // 1MHz 115200
      UCA0MCTL |= UCBRS_1 + UCBRF_0;            // Modulation UCBRSx=1, UCBRFx=0
      UCA0CTL1 &= ~UCSWRST;                     // **Initialize USCI state machine**
      UCA0IE |= UCRXIE;                         // Enable USCI_A0 RX interrupt
    
      __bis_SR_register(LPM0_bits + GIE);       // Enter LPM0, interrupts enabled
      __no_operation();                         // For debugger
    }
    
    // Echo back RXed character, confirm TX buffer is ready first
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=USCI_A0_VECTOR
    __interrupt void USCI_A0_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      switch(__even_in_range(UCA0IV,4))
      {
      case 0:break;                             // Vector 0 - no interrupt
      case 2:                                   // Vector 2 - RXIFG
        while (!(UCA0IFG&UCTXIFG));             // USCI_A0 TX buffer ready?
        UCA0TXBUF = UCA0RXBUF;                  // TX -> RXed character
        break;
      case 4:break;                             // Vector 4 - TXIFG
      default: break;
      }
    }
    
  • TI评估板本身就带USB转串口,完全可以利用这个做数据上传。

    在电脑属性中可以找到这个COM编号。

  • 这个程序我试过了,在数据传输时,单片机和电脑都没有反应,开发板是不是不能直接通过UART给上位机传输数据,只能通过USB转串口这种方法

  • 数据传输的的时候,只能是USB转串口,不能直接用串口发送吗

  •  电脑的串口 是 RS232 电平  单片机的 串口是 TTL 电平,两者不能直接通讯 , 需要电平转换。

    请补充一下基础知识~

  • 所以必须要通过开发板里面的USB转串口才能实现数据的传输,是这样吗

  • 通过开发板里面的USB转串口实现数据的传输 是最简便的方法

    当然你也可以用其他的USB转串口设备,原理是一样的