在网上看到一篇高精度测频模块论文,我改了一下 ,在闸门时间内,用F5529TA2CCR0捕获测频,可是好像有很大问题,一是捕获值会出现负值,不应该是在0-65535内吗?二是频率误差非常大,不知道为什么?这是我修改的代码,希望大家探讨指点。#include <msp430f5529.h>
#include <stdint.h>
#include <stdio.h>
#include "Dogs102x6.h"
#define CPUF ((double)1048576)
#define delay_us(x) __delay_cycles((long)(CPUF*(double)x/1000000))
#define delay_ms(x) __delay_cycles((long)(CPUF*(double)x/1000))
#define delay_s(x) __delay_cycles(CPUF*x)
#define ulint unsigned long int
/*
* main.c
*/
ulint captar=0,pulse=0,time=0,capfirst,caplast,flag=0,f;
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // 关闭看门狗
lcdinit();
P2DIR &= ~BIT3;
P2SEL |=BIT3;
TA2CCTL0=CM_1+SCS+CCIS_0+CAP+CCIE;
TA2CTL=TASSEL_1+MC_2+TAIE;
_EINT();
while(1){
if(flag==1){
f=pulse*32768/time;
display(f);//显示程序
flag=0;
}
}
}
#pragma vector = TIMER2_A0_VECTOR
__interrupt void TIMER2_A0 (void)
{
if(captar==0)//第一次捕获上升沿
{
capfirst=TA2CCR0;
captar++;
}
else{
caplast=TA2CCR0;
captar++;
}
}
#pragma vector = TIMER2_A1_VECTOR
__interrupt void TIMER2_A1 (void)
{
//TA2CTL&=~TAIE;
switch(TA2IV){
case 14:{//开启闸门时间2s;
if(captar==0)
pulse=0;
else{
//TA2CTL&= ~TAIE;
pulse=captar-1;待测信号个数
time=caplast-capfirst;标准信号个数
captar=0;
flag=1;//置位标志
}
break;
}
default:break;
}
//TA2CTL |= TAIE;
}
这是我参考的网上资料wenku.baidu.com/link