This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp432使用i2c_master_w_multibyte-master_code例程修改为使用EUSCI_B3时的问题



msp432使用i2c_master_w_multibyte-master_code例程修改为使用EUSCI_B3时,如下配置中断向量正确么?

extern void EUSCIB3_IRQHandler (void);
/* Interrupt vector table.  Note that the proper constructs must be placed on this to  */
/* ensure that it ends up at physical address 0x0000.0000 or at the start of          */
/* the program if located at a start address other than 0.                            */
#pragma RETAIN(interruptVectors)
#pragma DATA_SECTION(interruptVectors, ".intvecs")
void (* const interruptVectors[])(void) =
{
    (void (*)(void))((uint32_t)&__STACK_END),
                                            /* The initial stack pointer */
    resetISR,                               /* The reset handler         */
    nmiISR,                                 /* The NMI handler           */
    faultISR,                               /* The hard fault handler    */
    defaultISR,                             /* The MPU fault handler     */
    defaultISR,                             /* The bus fault handler     */
    defaultISR,                             /* The usage fault handler   */
    0,                                      /* Reserved                  */
    0,                                      /* Reserved                  */
    0,                                      /* Reserved                  */
    0,                                      /* Reserved                  */
    defaultISR,                             /* SVCall handler            */
    defaultISR,                             /* Debug monitor handler     */
    0,                                      /* Reserved                  */
    defaultISR,                             /* The PendSV handler        */
    defaultISR,                             /* The SysTick handler       */
    defaultISR,                             /* PSS ISR                   */
    defaultISR,                             /* CS ISR                    */
    defaultISR,                             /* PCM ISR                   */
    defaultISR,                             /* WDT ISR                   */
    defaultISR,                             /* FPU ISR                   */
    defaultISR,                             /* FLCTL ISR                 */
    defaultISR,                             /* COMP0 ISR                 */
    defaultISR,                             /* COMP1 ISR                 */
    defaultISR,                             /* TA0_0 ISR                 */
    defaultISR,                             /* TA0_N ISR                 */
    defaultISR,                             /* TA1_0 ISR                 */
    defaultISR,                             /* TA1_N ISR                 */
    defaultISR,                             /* TA2_0 ISR                 */
    defaultISR,                             /* TA2_N ISR                 */
    defaultISR,                             /* TA3_0 ISR                 */
    defaultISR,                             /* TA3_N ISR                 */
    defaultISR,                             /* EUSCIA0 ISR               */
    defaultISR,                             /* EUSCIA1 ISR               */
    defaultISR,                             /* EUSCIA2 ISR               */
    defaultISR,                             /* EUSCIA3 ISR               */
 defaultISR,                     /* EUSCIB0 ISR               */
    defaultISR,                             /* EUSCIB1 ISR               */
    defaultISR,                             /* EUSCIB2 ISR               */
 EUSCIB3_IRQHandler,                             /* EUSCIB3 ISR               */
    defaultISR,                             /* ADC14 ISR                 */
    defaultISR,                             /* T32_INT1 ISR              */
    defaultISR,                             /* T32_INT2 ISR              */
    defaultISR,                             /* T32_INTC ISR              */
    defaultISR,                             /* AES ISR                   */
    defaultISR,                             /* RTC ISR                   */
    defaultISR,                             /* DMA_ERR ISR               */
    defaultISR,                             /* DMA_INT3 ISR              */
    defaultISR,                             /* DMA_INT2 ISR              */
    defaultISR,                             /* DMA_INT1 ISR              */
    defaultISR,                             /* DMA_INT0 ISR              */
    defaultISR,                             /* PORT1 ISR                 */
    defaultISR,                             /* PORT2 ISR                 */
    defaultISR,                             /* PORT3 ISR                 */
    defaultISR,                             /* PORT4 ISR                 */
    defaultISR,                             /* PORT5 ISR                 */
    defaultISR,                             /* PORT6 ISR                 */
    defaultISR,                             /* Reserved 41               */
    defaultISR,                             /* Reserved 42               */
    defaultISR,                             /* Reserved 43               */
    defaultISR,                             /* Reserved 44               */
    defaultISR,                             /* Reserved 45               */
    defaultISR,                             /* Reserved 46               */
    defaultISR,                             /* Reserved 47               */
    defaultISR,                             /* Reserved 48               */
    defaultISR,                             /* Reserved 49               */
    defaultISR,                             /* Reserved 50               */
    defaultISR,                             /* Reserved 51               */
    defaultISR,                             /* Reserved 52               */
    defaultISR,                             /* Reserved 53               */
    defaultISR,                             /* Reserved 54               */
    defaultISR,                             /* Reserved 55               */
    defaultISR,                             /* Reserved 56               */
    defaultISR,                             /* Reserved 57               */
    defaultISR,                             /* Reserved 58               */
    defaultISR,                             /* Reserved 59               */
    defaultISR,                             /* Reserved 60               */
    defaultISR,                             /* Reserved 61               */
    defaultISR,                             /* Reserved 62               */
    defaultISR                              /* Reserved 63               */
};