使用IAR时,编译没有警告问题,使用CCS5.2时,出现好多警告!不过倒是还能执行调试,就是看到一堆警告不爽! 不解其中缘由,求帮助! 源程序如下:
#include <msp430.h>
void main( )
{
WDTCTL = WDTPW + WDTHOLD;
P1DIR |= 0x01;
for(;;)
{volatile unsigned int i;
P1OUT ^= 0x01;
i = 10000;
do i--;
while(i != 0);
}
}
编译的警告信息为:
#10374-D</a> Interrupt vector "ADC10" does not have an interrupt handler routine. lnk_msp430g2553.cmd /led line 82 C/C++ Problem
#10374-D</a> Interrupt vector "COMPARATORA" does not have an interrupt handler routine. lnk_msp430g2553.cmd /led line 88 C/C++ Problem
#10374-D</a> Interrupt vector "NMI" does not have an interrupt handler routine. lnk_msp430g2553.cmd /led line 91 C/C++ Problem
#10374-D</a> Interrupt vector "PORT1" does not have an interrupt handler routine. lnk_msp430g2553.cmd /led line 79 C/C++ Problem
#10374-D</a> Interrupt vector "PORT2" does not have an interrupt handler routine. lnk_msp430g2553.cmd /led line 80 C/C++ Problem
... 等等