This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430g2553



//******************************************************************************

//  MSP430F20xx Demo - Timer_A, Toggle P1.0-2, Cont. Mode ISR, 32kHz ACLK

//

//  Description: Use Timer_A CCRx units and overflow to generate four

//  independent timing intervals. For demonstration, CCR0 and CCR1 output

//  units are optionally selected with port pins P1.1 and P1.2 in toggle

//  mode. As such, these pins will toggle when respective CCRx registers match

//  the TAR counter. Interrupts are also enabled with all CCRx units,

//  software loads offset to next interval only - as long as the interval offset

//  is aded to CCRx, toggle rate is generated in hardware. Timer_A overflow ISR

//  is used to toggle P1.0 with software. Proper use of TAIV interrupt vector

//  generator is demonstrated.

//  ACLK = TACLK = 32kHz, MCLK = SMCLK = Default DCO

//  As coded and with TACLK = 32768Hz, toggle rates are:

//  P1.1 = CCR0 = 32768/(2*4) = 4096Hz

//  P1.2 = CCR1 = 32768/(2*16) = 1024Hz

//  P1.0 = overflow = 32768/(2*65536) = 0.25Hz

//  //* External watch crystal on XIN XOUT is required for ACLK *//

//

//              MSP430F20xx

//            ---------------

//        /|\|            XIN|-

//         | |               | 32kHz

//         --|RST        XOUT|-

//           |               |

//           |       P1.1/TA0|--> CCR0

//           |       P1.2/TA1|--> CCR1

//           |           P1.0|--> Overflow/software

//

//  M. Buccini / L. Westlund

//  Texas Instruments Inc.

//  October 2005

//  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.40A

//******************************************************************************

#include  <msp430x20x3.h>

void main(void)

{

 WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT

 P1SEL |= 0x06;                            // P1.1 - P1.2 option select

 P1DIR |= 0x07;                            // P1.0 - P1.2 outputs

 CCTL0 = OUTMOD_4 + CCIE;                  // CCR0 toggle, interrupt enabled

 CCTL1 = OUTMOD_4 + CCIE;                  // CCR1 toggle, interrupt enabled

 TACTL = TASSEL_1 + MC_2 + TAIE;           // ACLK, contmode, interrupt enabled

 _BIS_SR(LPM3_bits + GIE);                 // Enter LPM3 w/interrupt

}

// Timer A0 interrupt service routine

#pragma vector=TIMERA0_VECTOR

__interrupt void Timer_A0 (void)

{

 CCR0 += 4;                                // Add Offset to CCR0

}

// Timer_A2 Interrupt Vector (TAIV) handler

#pragma vector=TIMERA1_VECTOR

__interrupt void Timer_A1(void)

{

 switch( TAIV )

 {

 case  2: CCR1 += 16;                      // Add Offset to CCR1

          break;

 case 10: P1OUT ^= 0x01;                   // Timer_A3 overflow

          break;

}

}

这个程序是什么意思?