This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

大虾们我的也是G2553的串口问题

Other Parts Discussed in Thread: MAX232, MSP430G2553

我用的是TI官网的列程。并且也把 里面的PI.1 和P1.2换了 外接MAX232和PC通信

//******************************************************************************

//  MSP430G2xx3 Demo - Timer_A, Ultra-Low Pwr UART 9600 Echo, 32kHz ACLK

//

//  Description: Use Timer_A CCR0 hardware output modes and SCCI data latch

//  to implement UART function @ 9600 baud. Software does not directly read and

//  write to RX and TX pins, instead proper use of output modes and SCCI data

//  latch are demonstrated. Use of these hardware features eliminates ISR

//  latency effects as hardware insures that output and input bit latching and

//  timing are perfectly synchronised with Timer_A regardless of other

//  software activity. In the Mainloop the UART function readies the UART to

//  receive one character and waits in LPM3 with all activity interrupt driven.

//  After a character has been received, the UART receive function forces exit

//  from LPM3 in the Mainloop which configures the port pins (P1 & P2) based

//  on the value of the received byte (i.e., if BIT0 is set, turn on P1.0).

//  ACLK = TACLK = LFXT1 = 32768Hz, MCLK = SMCLK = default DCO

//  //* An external watch crystal is required on XIN XOUT for ACLK *//  

//

//               MSP430G2xx3

//            -----------------

//        /|\|              XIN|-

//         | |                 | 32kHz

//         --|RST          XOUT|-

//           |                 |

//           |   CCI0B/TXD/P1.1|-------->

//           |                 | 9600 8N1

//           |   CCI0A/RXD/P1.2|<--------

//

//  D. Dang

//  Texas Instruments Inc.

//  December 2010

//   Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10

//******************************************************************************

#include "msp430g2553.h"

//------------------------------------------------------------------------------

// Hardware-related definitions

//------------------------------------------------------------------------------

#define UART_RXD   0x02                     // TXD on P1.1 (Timer0_A.OUT0)

#define UART_TXD   0x04                     // RXD on P1.2 (Timer0_A.CCI1A)

//------------------------------------------------------------------------------

// Conditions for 9600 Baud SW UART, SMCLK = 1MHz

//------------------------------------------------------------------------------

#define UART_TBIT_DIV_2     (1000000 / (9600 * 2))

#define UART_TBIT           (1000000 / 9600)

//------------------------------------------------------------------------------

// Global variables used for full-duplex UART communication

//------------------------------------------------------------------------------

unsigned int txData;                        // UART internal variable for TX

unsigned char rxBuffer;                     // Received UART character

//------------------------------------------------------------------------------

// Function prototypes

//------------------------------------------------------------------------------

void TimerA_UART_init(void);

void TimerA_UART_tx(unsigned char byte);

void TimerA_UART_print(char *string);

//------------------------------------------------------------------------------

// main()

//------------------------------------------------------------------------------

void main(void)

{

   WDTCTL = WDTPW + WDTHOLD;               // Stop watchdog timer

   DCOCTL = 0x00;                          // Set DCOCLK to 1MHz

   BCSCTL1 = CALBC1_1MHZ;

   DCOCTL = CALDCO_1MHZ;

   P1OUT = 0x00;                           // Initialize all GPIO

   P1SEL = UART_TXD + UART_RXD;            // Timer function for TXD/RXD pins

   P1DIR = 0x00 & ~UART_RXD;               // Set all pins but RXD to output

   P2OUT = 0x00;

   P2SEL = 0x00;

   P2DIR = 0xFF;

   __enable_interrupt();

   TimerA_UART_init();                     // Start Timer_A UART

   TimerA_UART_print("G2xx2 TimerA UART\r\n");

   TimerA_UART_print("READY.\r\n");

   for (;;)

   {

       // Wait for incoming character

       __bis_SR_register(LPM0_bits);

       // Update board outputs according to received byte

       if (rxBuffer & 0x01) P1OUT |= 0x01; else P1OUT &= ~0x01;    // P1.0

       if (rxBuffer & 0x02) P1OUT |= 0x08; else P1OUT &= ~0x08;    // P1.3

       if (rxBuffer & 0x04) P1OUT |= 0x10; else P1OUT &= ~0x10;    // P1.4

       if (rxBuffer & 0x08) P1OUT |= 0x20; else P1OUT &= ~0x20;    // P1.5

       if (rxBuffer & 0x10) P1OUT |= 0x40; else P1OUT &= ~0x40;    // P1.6

       if (rxBuffer & 0x20) P1OUT |= 0x80; else P1OUT &= ~0x80;    // P1.7

       if (rxBuffer & 0x40) P2OUT |= 0x40; else P2OUT &= ~0x40;    // P2.6

       if (rxBuffer & 0x80) P2OUT |= 0x80; else P2OUT &= ~0x80;    // P2.7

       // Echo received character

       TimerA_UART_tx(rxBuffer);

   }

}

//------------------------------------------------------------------------------

// Function configures Timer_A for full-duplex UART operation

//------------------------------------------------------------------------------

void TimerA_UART_init(void)

{

   TACCTL0 = OUT;                          // Set TXD Idle as Mark = '1'

   TACCTL1 = SCS + CM1 + CAP + CCIE;       // Sync, Neg Edge, Capture, Int

   TACTL = TASSEL_2 + MC_2;                // SMCLK, start in continuous mode

}

//------------------------------------------------------------------------------

// Outputs one byte using the Timer_A UART

//------------------------------------------------------------------------------

void TimerA_UART_tx(unsigned char byte)

{

   while (TACCTL0 & CCIE);                 // Ensure last char got TX'd

   TACCR0 = TAR;                           // Current state of TA counter

   TACCR0 += UART_TBIT;                    // One bit time till first bit

   TACCTL0 = OUTMOD0 + CCIE;               // Set TXD on EQU0, Int

   txData = byte;                          // Load global variable

   txData |= 0x100;                        // Add mark stop bit to TXData

   txData <<= 1;                           // Add space start bit

}

//------------------------------------------------------------------------------

// Prints a string over using the Timer_A UART

//------------------------------------------------------------------------------

void TimerA_UART_print(char *string)

{

   while (*string) {

       TimerA_UART_tx(*string++);

   }

}

//------------------------------------------------------------------------------

// Timer_A UART - Transmit Interrupt Handler

//------------------------------------------------------------------------------

#pragma vector = TIMER0_A0_VECTOR

__interrupt void Timer_A0_ISR(void)

{

   static unsigned char txBitCnt = 10;

   TACCR0 += UART_TBIT;                    // Add Offset to CCRx

   if (txBitCnt == 0) {                    // All bits TXed?

       TACCTL0 &= ~CCIE;                   // All bits TXed, disable interrupt

       txBitCnt = 10;                      // Re-load bit counter

   }

   else {

       if (txData & 0x01) {

         TACCTL0 &= ~OUTMOD2;              // TX Mark '1'

       }

       else {

         TACCTL0 |= OUTMOD2;               // TX Space '0'

       }

       txData >>= 1;

       txBitCnt--;

   }

}      

//------------------------------------------------------------------------------

// Timer_A UART - Receive Interrupt Handler

//------------------------------------------------------------------------------

#pragma vector = TIMER0_A1_VECTOR

__interrupt void Timer_A1_ISR(void)

{

   static unsigned char rxBitCnt = 8;

   static unsigned char rxData = 0;

   switch (__even_in_range(TA0IV, TA0IV_TAIFG)) { // Use calculated branching

       case TA0IV_TACCR1:                        // TACCR1 CCIFG - UART RX

           TACCR1 += UART_TBIT;                 // Add Offset to CCRx

           if (TACCTL1 & CAP) {                 // Capture mode = start bit edge

               TACCTL1 &= ~CAP;                 // Switch capture to compare mode

               TACCR1 += UART_TBIT_DIV_2;       // Point CCRx to middle of D0

           }

           else {

               rxData >>= 1;

               if (TACCTL1 & SCCI) {            // Get bit waiting in receive latch

                   rxData |= 0x80;

               }

               rxBitCnt--;

               if (rxBitCnt == 0) {             // All bits RXed?

                   rxBuffer = rxData;           // Store in global variable

                   rxBitCnt = 8;                // Re-load bit counter

                   TACCTL1 |= CAP;              // Switch compare to capture mode

                   __bic_SR_register_on_exit(LPM0_bits);  // Clear LPM0 bits from 0(SR)

               }

           }

           break;

   }

}

//------------------------------------------------------------------------------

为什么通信时我接收总是出问题