This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5418的RTC设置问题



使用RTC实现日历功能,BCD编码格式。在设置月份和天的时候会出现写不进去(寄存器值不变)。初始化代码如下:

void Init_Rtc(void)
{
RTCCTL01 = RTCBCD + RTCHOLD + RTCMODE + RTCTEV_0 ;// BCD码日历格式输出
RTCPS0CTL = RT0PSHOLD ; //配置两个计数器分频
RTCPS1CTL = RT1PSHOLD ;
if(RTCYEAR<0x2015||RTCYEAR>0x2050)
{
RTCSEC = g_now.Sec; //初始化秒
RTCMIN = g_now.Min ; //初始化分钟
RTCHOUR =g_now.Hour; //初始化小时
RTCDOW = 0X04 ;
RTCDAY = g_now.Day; //日期初始化
RTCMON = g_now.Month ; //初始化月份
RTCYEAR = g_now.Year; //初始化年份
}
RTCCTL01 &= ~RTCHOLD; //打开RTC模块
RTCPS0CTL &= ~RT0PSHOLD; //打开RTCPS0CTL
RTCPS1CTL &= ~RT1PSHOLD; //打开RTCPS1CTL
RTCCTL0 |= RTCAIE;
RTCCTL1 &= ~(RTCHOLD);
}

  • 参考以下例程试试先

    /* --COPYRIGHT--,BSD_EX
    * Copyright (c) 2012, Texas Instruments Incorporated
    * All rights reserved.
    *
    * Redistribution and use in source and binary forms, with or without
    * modification, are permitted provided that the following conditions
    * are met:
    *
    * * Redistributions of source code must retain the above copyright
    * notice, this list of conditions and the following disclaimer.
    *
    * * Redistributions in binary form must reproduce the above copyright
    * notice, this list of conditions and the following disclaimer in the
    * documentation and/or other materials provided with the distribution.
    *
    * * Neither the name of Texas Instruments Incorporated nor the names of
    * its contributors may be used to endorse or promote products derived
    * from this software without specific prior written permission.
    *
    * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
    * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
    * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
    * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
    * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
    * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
    * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
    * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
    * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
    * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
    * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    *
    *******************************************************************************
    *
    * MSP430 CODE EXAMPLE DISCLAIMER
    *
    * MSP430 code examples are self-contained low-level programs that typically
    * demonstrate a single peripheral function or device feature in a highly
    * concise manner. For this the code may rely on the device's power-on default
    * register values and settings such as the clock configuration and care must
    * be taken when combining code from several examples to avoid potential side
    * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
    * for an API functional library-approach to peripheral configuration.
    *
    * --/COPYRIGHT--*/
    //******************************************************************************
    // MSP430F54xA Demo - RTC_A in real time clock mode
    //
    // Description: This program demonstrates the RTC mode by triggering an
    // interrupt every second and minute. This code toggles P1.0 every second.
    // This code recommends an external LFXT1 crystal for RTC accuracy.
    // ACLK = LFXT1 = 32768Hz, MCLK = SMCLK = default DCO = 32 x ACLK = 1048576Hz
    //
    // MSP430F54xA
    // -----------------
    // /|\ | XIN|-
    // | | | 32kHz
    // ---|RST XOUT|-
    // | |
    // | P1.0 |--> Toggles every second
    // | |
    //
    // W. Goh
    // Texas Instruments Inc.
    // April 2010
    // Built with CCS version 4.2 and IAR Embedded Workbench Version: 4.21.8
    //******************************************************************************

    #include <msp430.h>

    int main(void)
    {
    WDTCTL = WDTPW + WDTHOLD; // Stop Watchdog Timer
    P1DIR |= BIT0; // Set P1.0 as output

    // Initialize LFXT1
    P7SEL |= 0x03; // Select XT1
    UCSCTL6 &= ~(XT1OFF); // XT1 On
    UCSCTL6 |= XCAP_3; // Internal load cap

    // Loop until XT1,XT2 & DCO fault flag is cleared
    do
    {
    UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + XT1HFOFFG + DCOFFG);
    // Clear XT2,XT1,DCO fault flags
    SFRIFG1 &= ~OFIFG; // Clear fault flags
    }while (SFRIFG1&OFIFG); // Test oscillator fault flag

    // Configure RTC_A
    RTCCTL01 |= RTCTEVIE + RTCRDYIE + RTCBCD + RTCHOLD + RTCMODE;
    // RTC enable, BCD mode, RTC hold
    // enable RTC read ready interrupt
    // enable RTC time event interrupt

    RTCYEAR = 0x2010; // Year = 0x2010
    RTCMON = 0x4; // Month = 0x04 = April
    RTCDAY = 0x05; // Day = 0x05 = 5th
    RTCDOW = 0x01; // Day of week = 0x01 = Monday
    RTCHOUR = 0x10; // Hour = 0x10
    RTCMIN = 0x32; // Minute = 0x32
    RTCSEC = 0x45; // Seconds = 0x45

    RTCADOWDAY = 0x2; // RTC Day of week alarm = 0x2
    RTCADAY = 0x20; // RTC Day Alarm = 0x20
    RTCAHOUR = 0x10; // RTC Hour Alarm
    RTCAMIN = 0x23; // RTC Minute Alarm

    RTCCTL01 &= ~(RTCHOLD); // Start RTC calendar mode

    __bis_SR_register(LPM3_bits + GIE); // Enter LPM3 mode with interrupts
    // enabled
    __no_operation();
    }

    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=RTC_VECTOR
    __interrupt void RTC_ISR(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(RTC_VECTOR))) RTC_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
    switch(__even_in_range(RTCIV,16))
    {
    case RTC_NONE: // No interrupts
    break;
    case RTC_RTCRDYIFG: // RTCRDYIFG
    P1OUT ^= 0x01; // Toggles P1.0 every second
    break;
    case RTC_RTCTEVIFG: // RTCEVIFG
    __no_operation(); // Interrupts every minute
    break;
    case RTC_RTCAIFG: // RTCAIFG
    break;
    case RTC_RT0PSIFG: // RT0PSIFG
    break;
    case RTC_RT1PSIFG: // RT1PSIFG
    break;
    case 12: break; // Reserved
    case 14: break; // Reserved
    case 16: break; // Reserved
    default: break;
    }
    }

  • 中断处理函数用来做什么的?还有就是,经常存不进去,写改变不了。

  • 你都已经用Struct,贴一下g_now的结构呢?

    driverlib 里有个和你这个类似的Calendar 结构,建议你用driverlib。

  • 结构体是这样定义的:

    typedef struct
    {
    unsigned int Year;
    unsigned char Month;
    unsigned char Day;
    unsigned char Hour;
    unsigned char Min;
    unsigned char Sec;
    }DateTime;