This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于bootloader demo的疑问

TI官方自带的bootloader Demo,app proxy interrupt table里中断向量地址前面加了个BRA instruction (0x4030)。请问这个BRA instruction (0x4030)是什么指令?为什么要加入到中断向量表中的地址前面呢?

//
//  Constant tables
//
/*! This is a "proxy" interrupt table which is used by the bootloader to jump to
    each interrupt routine.
    It always resides in the same location.
    It contains a BRA instruction (0x4030) followed by the address of each
    vector routine.
    Note that the number and location of each vector should match the declaration
    in Boot's Vector_Table (TI_MSPBoot_VecRed_G2xxxx.c)
    Unimplemented vectors are removed (and unused vectors can be removed too)
    to save flash space
    The following table matches the vectors for G2553
*/
#   ifdef __IAR_SYSTEMS_ICC__
#       pragma location="APP_PROXY_VECTORS"
__root const uint16_t ProxyVectorTable[] =
#   elif defined (__TI_COMPILER_VERSION__)
#       pragma DATA_SECTION(ProxyVectorTable, ".APP_PROXY_VECTORS")
#       pragma RETAIN(ProxyVectorTable)
const uint16_t ProxyVectorTable[] =
#   endif
{
        0x4030, (uint16_t) P1_Isr,              // APP_PROXY_VECTOR(0) P1
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(1) P2
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(2) ADC10
        0x4030, (uint16_t) TI_MSPBoot_Comm_Isr,   // APP_PROXY_VECTOR(3) USCI I2C TX/RX
        0x4030, (uint16_t) TI_MSPBoot_Comm_Isr, // APP_PROXY_VECTOR(4) USCI I2C STAT
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(5) TA0_1
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(6) T0_0
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(7) WDT
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(8) COMP_A
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(9) TA1_1
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(10) TA1_0
        0x4030, (uint16_t) Dummy_Isr,           // APP_PROXY_VECTOR(11) NMI
};