锂电池供电时,SVS开启,msp430f4152的flash擦除和写电压最低是2.2V;如果锂电池降到2.5V,RTC时间到了,需要刷flash info,会不会出现这种情况:flash info刷到一半,电压降到2.2V以下,SVS使单片机复位了,结果数据错的离谱。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
锂电池供电时,SVS开启,msp430f4152的flash擦除和写电压最低是2.2V;如果锂电池降到2.5V,RTC时间到了,需要刷flash info,会不会出现这种情况:flash info刷到一半,电压降到2.2V以下,SVS使单片机复位了,结果数据错的离谱。
3.6V的锂电池,可以直接接msp430,或者加一个LDO再接msp430。SVS我可以调到2.5V或2.65V甚至2.8V,擦除flash时,锂电会不会跌落0.5V以下,flash擦除或写操作还没完成,svs使单片机复位啊?
你可以开启ADC对电池电压进行监控,譬如电压低于3.0V时候不对FLASH进行操作,相差0.02V很难回答会不会复位。