This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430g2553 ADC10测量温度官方例程找不到

自带温度传感器测温度不会使用 找不到程序 还有就是想在数码管上显示测量结果 求助 谢谢!
  • /* --COPYRIGHT--,BSD_EX
     * Copyright (c) 2012, Texas Instruments Incorporated
     * All rights reserved.
     *
     * Redistribution and use in source and binary forms, with or without
     * modification, are permitted provided that the following conditions
     * are met:
     *
     * *  Redistributions of source code must retain the above copyright
     *    notice, this list of conditions and the following disclaimer.
     *
     * *  Redistributions in binary form must reproduce the above copyright
     *    notice, this list of conditions and the following disclaimer in the
     *    documentation and/or other materials provided with the distribution.
     *
     * *  Neither the name of Texas Instruments Incorporated nor the names of
     *    its contributors may be used to endorse or promote products derived
     *    from this software without specific prior written permission.
     *
     * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
     * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
     * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
     * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
     * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
     * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
     * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
     * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
     * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
     * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
     * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
     *
     *******************************************************************************
     * 
     *                       MSP430 CODE EXAMPLE DISCLAIMER
     *
     * MSP430 code examples are self-contained low-level programs that typically
     * demonstrate a single peripheral function or device feature in a highly
     * concise manner. For this the code may rely on the device's power-on default
     * register values and settings such as the clock configuration and care must
     * be taken when combining code from several examples to avoid potential side
     * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware
     * for an API functional library-approach to peripheral configuration.
     *
     * --/COPYRIGHT--*/
    //******************************************************************************
    //  MSP430G2x33/G2x53 Demo - ADC10, Sample A10 Temp and Convert to oC and oF
    //
    //  Description: A single sample is made on A10 with reference to internal
    //  1.5V Vref. Software sets ADC10SC to start sample and conversion - ADC10SC
    //  automatically cleared at EOC. ADC10 internal oscillator/4 times sample
    //  (64x) and conversion. In Mainloop MSP430 waits in LPM0 to save power until
    //  ADC10 conversion complete, ADC10_ISR will force exit from any LPMx in
    //  Mainloop on reti. Temperaure in oC stored in IntDegC, oF in IntDegF.
    //  Uncalibrated temperature measured from device to device will vary with
    //  slope and offset - please see datasheet.
    //  ACLK = n/a, MCLK = SMCLK = default DCO ~1.2MHz, ADC10CLK = ADC10OSC/4
    //
    //                MSP430G2x33/G2x53
    //             -----------------
    //         /|\|              XIN|-
    //          | |                 |
    //          --|RST          XOUT|-
    //            |                 |
    //            |A10              |
    //
    //  D. Dang
    //  Texas Instruments Inc.
    //  December 2010
    //   Built with CCS Version 4.2.0 and IAR Embedded Workbench Version: 5.10
    //******************************************************************************
    #include <msp430.h>
    
    long temp;
    long IntDegF;
    long IntDegC;
    
    int main(void)
    {
      WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT
      ADC10CTL1 = INCH_10 + ADC10DIV_3;         // Temp Sensor ADC10CLK/4
      ADC10CTL0 = SREF_1 + ADC10SHT_3 + REFON + ADC10ON + ADC10IE;
      __enable_interrupt();                     // Enable interrupts.
      TACCR0 = 30;                              // Delay to allow Ref to settle
      TACCTL0 |= CCIE;                          // Compare-mode interrupt.
      TACTL = TASSEL_2 | MC_1;                  // TACLK = SMCLK, Up mode.
      LPM0;                                     // Wait for delay.
      TACCTL0 &= ~CCIE;                         // Disable timer Interrupt
      __disable_interrupt();
    
      while(1)
      {
        ADC10CTL0 |= ENC + ADC10SC;             // Sampling and conversion start
        __bis_SR_register(CPUOFF + GIE);        // LPM0 with interrupts enabled
    
        // oF = ((A10/1024)*1500mV)-923mV)*1/1.97mV = A10*761/1024 - 468
        temp = ADC10MEM;
        IntDegF = ((temp - 630) * 761) / 1024;
    
        // oC = ((A10/1024)*1500mV)-986mV)*1/3.55mV = A10*423/1024 - 278
        temp = ADC10MEM;
        IntDegC = ((temp - 673) * 423) / 1024;
    
        __no_operation();                       // SET BREAKPOINT HERE
      }
    }
    
    // ADC10 interrupt service routine
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC10_VECTOR
    __interrupt void ADC10_ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC10_VECTOR))) ADC10_ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
      __bic_SR_register_on_exit(CPUOFF);        // Clear CPUOFF bit from 0(SR)
    }
    
    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=TIMER0_A0_VECTOR
    __interrupt void ta0_isr(void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) ta0_isr (void)
    #else
    #error Compiler not supported!
    #endif
    {
      TACTL = 0;
      LPM0_EXIT;                                // Exit LPM0 on return
    }