This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

msp430f149外部5路ad转换,程序这样写没用作用。希望大家指点,急急!!!

#include <msp430x14x.h>
#include "TA.c"
#include "direction.c"
#include "Key.c"


#define uchar unsigned char
#define uint unsigned int


uint Red_distance;
uint Optic_reflect;
static unsigned int results[5];
uint vth = 0x000f ;
uint adc_flag=0;

void int_AD()
{
P6SEL = 0x001F; // Enable A/D channel inputs
ADC12CTL0 = ADC12ON+MSC+SHT0_2; // Turn on ADC12, set sampling time
ADC12CTL1 = SHP+CONSEQ_1; // Use sampling timer, single sequence
ADC12MCTL0 = INCH_0; // ref+=AVcc, channel = A0
ADC12MCTL1 = INCH_1; // ref+=AVcc, channel = A1
ADC12MCTL2 = INCH_2; // ref+=AVcc, channel = A2
ADC12MCTL3 = INCH_3; // ref+=AVcc, channel = A3
ADC12MCTL4 = INCH_4+EOS; // ref+=AVcc, channel = A4, end seq.
ADC12IE = 0x0001; // Enable ADC12IFG.3
ADC12CTL0 |= ENC; // Enable conversions

}

void main()
{
uint i,k=0;

WDTCTL = WDTPW + WDTHOLD;
int_clk();
TAPwmInit('A',1,'P','P'); //将定时器TA初始化成为PWM发生器
//时钟源=ACLK ; 无分频; 通道1和通道2均设为高电平模式。
TAPwmSetPeriod(1000); //通道1/2的PWM方波周期均设为500个时钟周期

P2DIR = 0X00FF;
Go_ahead(800,800);
P6DIR = 0X0000;
P5DIR = 0X0000;
P4DIR = 0X0001;
P4OUT = 0X0000;
int_AD();
ADC12CTL0 |= ADC12SC; // Start conversion
_EINT();

while(1)
{
Go_ahead(800,800);
Red_distance = P5IN & 0x00F8; //蔽障
Delay_Nms(4);
Red_distance = P5IN&0x00F8;
//ADC12CTL0 |= ADC12SC; //启动ad转换
// for(i=0;i<5;i++)
//if(results[i] > vth)
//{
//k = 1;
//}
//if(k == 1) Stop();
//if(k == 0)
//{
if(Red_distance != 0x00F8)
{
Red_Key(Red_distance);
k=0;
}
else
{
ADC12CTL0 |= ADC12SC; // Start conversion
Delay_Nms(1);
Optic_zuobiao(results[0],results[1],results[2],results[3],results[4]);
k=0;
}
}
/* if(adc_flag == 1)
{
ADC12CTL0 |= ADC12SC;
adc_flag=0;
}*/
// Red_Key(Red_distance);
// Red_reflect = jisuan(Red_reflect);
// PID_Control(uchar Position)
//}
}

#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=ADC12_VECTOR
__interrupt void ADC12ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
#else
#error Compiler not supported!
#endif
{
results[0] = ADC12MEM0; // Move results, IFG is cleared
results[1] = ADC12MEM1; // Move results, IFG is cleared
results[2] = ADC12MEM2; // Move results, IFG is cleared
results[3] = ADC12MEM3; // Move results, IFG is cleared
results[4] = ADC12MEM4; // Move results, IFG is cleared

//adc_flag=1;
//__bic_SR_register_on_exit(LPM0_bits); // Clear LPM0, SET BREAKPOINT HERE
}

  • adc12是逐个通道依次转换的。建议参考下官网提供的例程

  • #include <msp430.h>

    static unsigned int results[4]; // Needs to be global in this example
    // Otherwise, the compiler removes it
    // because it is not used for anything.

    int main(void)
    {
    WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer
    P6SEL = 0x0F; // Enable A/D channel inputs
    ADC12CTL0 = ADC12ON+MSC+SHT0_2; // Turn on ADC12, set sampling time
    ADC12CTL1 = SHP+CONSEQ_1; // Use sampling timer, single sequence
    ADC12MCTL0 = INCH_0; // ref+=AVcc, channel = A0
    ADC12MCTL1 = INCH_1; // ref+=AVcc, channel = A1
    ADC12MCTL2 = INCH_2; // ref+=AVcc, channel = A2
    ADC12MCTL3 = INCH_3+EOS; // ref+=AVcc, channel = A3, end seq.
    ADC12IE = 0x08; // Enable ADC12IFG.3
    ADC12CTL0 |= ENC; // Enable conversions

    while(1)
    {
    ADC12CTL0 |= ADC12SC; // Start conversion
    __bis_SR_register(LPM0_bits + GIE); // Enter LPM0, Enable interrupts
    }
    }

    #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
    #pragma vector=ADC12_VECTOR
    __interrupt void ADC12ISR (void)
    #elif defined(__GNUC__)
    void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void)
    #else
    #error Compiler not supported!
    #endif
    {
    results[0] = ADC12MEM0; // Move results, IFG is cleared
    results[1] = ADC12MEM1; // Move results, IFG is cleared
    results[2] = ADC12MEM2; // Move results, IFG is cleared
    results[3] = ADC12MEM3; // Move results, IFG is cleared
    __bic_SR_register_on_exit(LPM0_bits); // Clear LPM0, SET BREAKPOINT HERE
    }

    这个是官网提供的程序。不知道我的有什么问题。