This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F247的I2C的使用方法



如何设置相关寄存器?有例程可供参考吗?

  • TI有相应的Code Example,希望您可以参考TI的例程,这样可以节省很多的开发时间和学习时间

  • //******************************************************************************

    //  MSP430F21x2 Demo - USCI_B0 I2C Master RX single bytes from MSP430 Slave

    //

    //  Description: This demo connects two MSP430's via the I2C bus. The master

    //  reads from the slave. This is the master code. The data from the slave

    //  transmitter begins at 0 and increments with each transfer. The received

    //  data is in R5 and is checked for validity. If the received data is

    //  incorrect, the CPU is trapped and the P1.0 LED will stay on. The USCI_B0

    //  RX interrupt is used to know when new data has been received.

    //  ACLK = n/a, MCLK = SMCLK = BRCLK = default DCO = ~1.2MHz

    //

    //                                /|\  /|\

    //               MSP430F21x2      10k  10k     MSP430F21x2

    //                   slave         |    |        master

    //             -----------------   |    |  -----------------

    //           -|XIN  P3.1/UCB0SDA|<-|---+->|P3.1/UCB0SDA  XIN|-

    //            |                 |  |      |                 | 32kHz

    //           -|XOUT             |  |      |             XOUT|-

    //            |     P3.2/UCB0SCL|<-+----->|P3.2/UCB0SCL     |

    //            |                 |         |             P1.0|--> LED

    //

    //  Andreas Dannenberg

    //  Texas Instruments Inc.

    //  October 2006

    //  Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.41A

    //******************************************************************************

    #include "msp430x21x2.h"

    unsigned char RXData;

    unsigned char RXCompare;

    void main(void)

    {

     WDTCTL = WDTPW + WDTHOLD;                 // Stop WDT

     P1OUT &= ~0x01;                           // P1.0 = 0

     P1DIR |= 0x01;                            // P1.0 output

     P3SEL |= 0x06;                            // Assign I2C pins to USCI_B0

     UCB0CTL1 |= UCSWRST;                      // Enable SW reset

     UCB0CTL0 = UCMST + UCMODE_3 + UCSYNC;     // I2C Master, synchronous mode

     UCB0CTL1 = UCSSEL_2 + UCSWRST;            // Use SMCLK, keep SW reset

     UCB0BR0 = 12;                             // fSCL = SMCLK/12 = ~100kHz

     UCB0BR1 = 0;

     UCB0I2CSA = 0x048;                        // Slave Address is 048h

     UCB0CTL1 &= ~UCSWRST;                     // Clear SW reset, resume operation

     IE2 |= UCB0RXIE;                          // Enable RX interrupt

     RXCompare = 0;                            // Used to check incoming data

     while (1)

     {

       while (UCB0CTL1 & UCTXSTP);             // Ensure stop condition got sent

       UCB0CTL1 |= UCTXSTT;                    // I2C start condition

       while (UCB0CTL1 & UCTXSTT);             // Start condition sent?

       UCB0CTL1 |= UCTXSTP;                    // I2C stop condition

       __bis_SR_register(CPUOFF + GIE);        // Enter LPM0 w/ interrupts

       if (RXData != RXCompare)                // Trap CPU if wrong

       {

         P1OUT |= 0x01;                        // P1.0 = 1

         while (1);                            // Trap CPU

       }

       RXCompare++;                            // Increment correct RX value

     }

    }

    // USCI_B0 Data ISR

    #pragma vector = USCIAB0TX_VECTOR

    __interrupt void USCIAB0TX_ISR(void)

    {

     RXData = UCB0RXBUF;                       // Get RX data

     __bic_SR_register_on_exit(CPUOFF);        // Exit LPM0

    }