This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI NFC评估板咨询~~



如下为具体的测试需求(从需求来看,不涉及协议测试这块),是否可以提供一些评估板型号以满足这些需求,谢谢~~

产品为非接触卡式 POS机,可实现NFC银行卡支付。支持标准:EMVCoL1

                  客户有两项测试内容:先满足A条件下再满足B

                  A:NFC感应距离测试;

                        NFC信号强度为正常6V时,频率为13.56Mhz时,要求测试线圈位于上方0cm和4cm(真实距离为0.5cm和4.5cm)的感应电压必须分别大于(含)6.0V和2.4V.

                  B :NFC信号MAX 显示干扰检测;

                        要求NFC信号开到MAX(8V),模组显示OK(不能有显示不良,例如白屏,画面异常等),不能有干扰。(客户会测试NFC信号强度6.5V、7.0V、7.5V和8V)