This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,我用msp430g2412的 P1.5(CA5)输入一个电压, P1.0(CA0)为输入的参考电压2.5v,比较它们的大小。但是不管P1.5的电压怎样变化,CAOUT都没有变化呢?这是怎么回事。
void main(void)
{
WDTCTL = WDTHOLD + WDTPW; // 关看门狗
// P1SEL |=BIT0+BIT5;
CAPD |=BIT0+BIT5;
P2DIR |=BIT2+BIT3+BIT4;
P2OUT |=BIT2+BIT4;
CACTL1 |= CAON+CAIE; //使用 CA0接P1.0 这2.5V参考电压
CACTL2 |= P2CA0+P2CA1+P2CA3; // 使用 CA5接P1.5 接比较电压
while(1)
{
if((CACTL2 & CAOUT))
{
if(i++>2000)
{
i=0;
P2OUT |=BIT3;
P2OUT ^=BIT4;
// CACTL1 |=CAEX;
}
}
else
{
if(i++>2000)
{
i=0;
P2OUT |=BIT4;
P2OUT ^=BIT3;
// CACTL1 &=~CAEX;
}
}
}
}
还是没的搞懂,我要的是两路都是外部输入。基准也是外部输入的。怎样同时选择CA0,CA5输入到+和-中。还有一个端口同时是比较器的输入和输出,怎样选择为输入。