如何从boot跳转到app,app 采用的是rtos系统?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
boot MAP
#define FLASH_BASE 0x00000000
#define BIM_BASE 0x00000000
#define BIM_FLASH_SIZE 0x2000
#define PAGE_SIZE 0x1000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x10000
#define APP_BASE 0x00002000
#define APP_FLASH_SIZE 0x00030000
MEMORY {
FLASH (RX) : origin = BIM_BASE, length = BIM_FLASH_SIZE
SRAM (RWX) : origin = RAM_BASE, length = 0x0000C800//length = 0x00002CFF
}
SECTIONS {
.intvecs: > BIM_BASE
.text : > FLASH
.const : > FLASH
.cinit : > FLASH
.pinit : > FLASH
.init_array : > FLASH
.flashMailbox : > 0x00200000
.vtable : > SRAM
.data : > SRAM
.bss : > SRAM
.sysmem : > SRAM
.stack : > SRAM (HIGH)
}
app MAP:
#ifndef APP_BASE #define APP_BASE 0x00002000
#endif //APP_BASE
#define FLASH_SIZE 0x40000
#define PAGE_SIZE 0x1000
#define RAM_BASE 0x20000000
#define RAM_SIZE 0x10000
#define APP_FLASH_MAX_SIZE 0x0003E000
MEMORY {
APP_FLASH (RX) : origin = APP_BASE, length = 0x0003E000
INFO (RX) : origin = 0x00200000, length = 0x00004000
SRAM_CODE (RWX): origin = 0x01000000, length = 0x00010000
SRAM_DATA (RW) : origin = 0x20000000, length = 0x00010000
}
SECTIONS {
// .intvecs: > APP_BASE
.text : > APP_FLASH
.const : > APP_FLASH
.cinit : > APP_FLASH
.pinit : > APP_FLASH
.init_array : > APP_FLASH
.resetVecs : > APP_BASE//+0x140
.flashMailbox : > 0x00200000
.vtable : > SRAM_DATA
.data : > SRAM_DATA
.bss : > SRAM_DATA
.sysmem : > SRAM_DATA
.stack : > SRAM_DATA (HIGH)
}